Por favor utilize outro browser (Google Chrome, Internet Explorer, Safari…)

Parece que está a usar um browser que não é totalmente compatível Por favor, note que podem haver restrições locais e usabilidade. Para uma melhor experiência, sugerimos que faça o download da versão mais recente de um browser compatível:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continuar com o browser atual

Power matters – especially for the oil and gas industry


Maximum safety, from the well to the customer

In the oil and gas business, power stability is essential for successful operation. System outages due to power failures or even minor disturbances in the power supply can have severe consequences. Processes and procedures demand maximum availability in power supply. Typically, oil and gas production sites are among the toughest and most dangerous environments. That’s why power matters – safety and security issues call for special attention.

TIP for oil and gas

A growing market with a steadily increasing need for power

While the world population continues to grow, so does the demand for oil and gas. In 2030, oil and gas will cater for 60% of the global energy demand, with ever more oil and gas used in power generation. At the same time, just about every upstream, midstream, or downstream oil and gas process requires reliable power.
And in the face of depleting wells, even more power will be needed for additional production techniques, such as depletion compression. Therefore, power supply must be efficient and reliable, even in remote locations, at all times. TIP solutions from Siemens focus on the unique economic and process requirements of this industry.

Major challenges for oil and gas

In the safety-critical oil and gas industry, space is usually extremely restricted and regulated by the most stringent safety regulations. In an effort to supply offshore power plants from the interconnected grid with power from the mainland, the industry is constantly looking for better solutions which address space needs, maintenance, and investment or personnel costs. And in times of digitalization, complex energy automation systems are being confronted with increasing demands. All components must work together smoothly, while the processes should remain transparent and available. A reliable power supply must always be ensured.

Our answer: Totally Integrated Power

Specific solutions for the oil and gas industry


Maximum reliability even under the most difficult conditions

For oil and gas production, electricity is a cost-intensive factor. That’s why Totally Integrated Power offers power solutions tailored to these requirements, which support the core tasks of the oil and gas industry with low space requirements, reliable performance under the toughest conditions, and maximum energy efficiency.

Increasing demands in times of digitization

Transparent energy consumption, optimal processes, and a smooth power supply: With its comprehensive energy automation portfolio, Totally Integrated Power offers cost-efficient energy management solutions at the highest level, featuring protection technology for energy systems and the control and automation of substations as well as remote monitoring and the measurement and recording of data.


Optimal protection for plants

Oil and gas production sites are among the harshest and most dangerous environments, and power stability is essential for their successful operation. System outages due to power failures or even minor disturbances in the power supply can have severe consequences.


Reliability and safety

Oil and gas production requires robust power supply solutions that ensure day-to-day reliability and availability of equipment in hostile environments. In addition, these solutions need to be safe, flexible, and cost-efficient – over the entire lifecycle.


Our TIP offerings in depth

Get to know our complete portfolio for power supply
TIP product portfolio


Successful use of TIP in the oil and gas industry

TIP is an integrated power supply solution that is being successfully used in the oil and gas industry around the world. Here are a number of reference projects.


Cost- and time-efficient in rough environments