Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens Mobility digitizes traffic in Wiesbaden

"This is a flagship project for Siemens Mobility. With our years of experience as experts in traffic engineering, we're making a strong contribution to clean air in Wiesbaden. This type of project is unique in Germany so far", said Manfred Fuhg, Head of Siemens Mobility Germany.
By using the levers of mobility, logistics and data, together with the active management of road traffic, traffic-related emissions in the city will be reduced. The system requires a large volume of data and information provided by cameras and sensors that quantitatively and anonymously monitor the traffic volumes of a variety of users such as vehicles, bicycles and pedestrians. Additional information covering public events, the city's mass transit systems and the changing parking situation is also included in the system's analysis, along with data provided by environmental sensors.
With the help of Big Data analytics, the flow of data from the various sources can be processed and linked. Correlations can then be determined from the analysed environmental and traffic data, and appropriate measures can be identified. These real-time analyses are the basis for active, environment-sensitive traffic controls.
Siemens Mobility is not only providing the infrastructure needed for the project, but will also employ simulation models provided by the recently integrated software company Aimsun.
For years, Wiesbaden has been one of the approximately 70 cities in Germany threatened by legal restrictions for diesel vehicles due to the regular exceeding of the limits set for nitrogen dioxide emissions.

For further information about Siemens Mobility, please see: www.siemens.com/mobility
Siemens Mobility is a separately managed company of Siemens AG. As a leader in transport solutions for more than 160 years, Siemens Mobility is constantly innovating its portfolio in its core areas of rolling stock, rail automation and electrification, turnkey systems, intelligent traffic systems as well as related services. With digitalization, Siemens Mobility is enabling mobility operators worldwide to make infrastructure intelligent, increase value sustainably over the entire lifecycle, enhance passenger experience and guarantee availability. In fiscal year 2018, which ended on September 30, 2018, the former Siemens Mobility Division posted revenue of €8.8 billion and had around 28,400 employees worldwide. Further information is available at: www.siemens.com/mobility.
Read more

Contact

Eva Haupenthal

Otto-Hahn-Ring 6
81739 Munich
Germany

+49 (89) 636-24421