Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

The world’s first HVDC transformer passes the test for ±1,100 kV level

The picture shows the world’s first ±1,100 kV HVDC transformer.

“With successful testing of the world’s first HVDC transformer for a transmission voltage of ± 1,100 kilovolts, we have set a new benchmark in direct-current transmission,” states Beatrix Natter, CEO of Power Transformers at Siemens Energy Management. “Experience and ingenuity are what made this development possible. It makes direct-current transmission over long distances more efficient for our customers, because higher transmission voltages mean lower transmission losses.”
The transformers will be installed in the Guquan converter station of the HVDC link between the Chinese cities of Changji (Xinjiang) and Guquan (Anhui). This is the world’s most powerful HVDC transmission system in terms of transmission capacity, voltage and length. It will transmit power with a DC voltage of ±1,100 kV for the first time anywhere in the world. The HVDC link is 3,324 kilometers long and will transmit electricity from the northwestern Xinjiang region to Anhui Province in eastern China. With a transmission capacity of twelve gigawatts (GW), it will replace what was previously the most powerful system with a capacity of 10 GW. In these systems, the transformers are used to feed power from conventional AC transmission grids into so-called converter stations. These generate the DC voltage on one side and convert it back to AC voltage on the receiving side. Due to the type of connection to the converters, the transformers will also be loaded with the very high DC quantities of the transmission voltage and current.
Based on many years of experience with HVDC transformers, Siemens further developed all key components of this type of transformer, thus reaching a new transmission level in HVDC technology. The workflows for manufacturing and testing this product were challenging due to the transformer’s extreme dimensions (LxWxH: 37.5 m x 12.0 m x 14.5 m). Nevertheless, the ±1,100 kV prototype was able to pass every test in terms of functionality, emissions and load level. The type-tested HVDC transformer is now being prepared for its long journey to China by road and sea.


Further information on Siemens-HVDC-Transformers
www.siemens.com/transformers
For further information on Division Energy Management, please see www.siemens.com/energy-management
Siemens AG (Berlin and Munich) is a global technology powerhouse that has stood for engineering excellence, innovation, quality, reliability and internationality for 170 years. The company is active in more than 200 countries, focusing on the areas of electrification, automation and digitalization. One of the world's largest producers of energy-efficient, resource-saving technologies, Siemens is a leading supplier of efficient power generation and power transmission solutions and a pioneer in infrastructure solutions as well as automation, drive and software solutions for industry. The company is also a leading provider of medical imaging equipment – such as computed tomography and magnetic resonance imaging systems – and a leader in laboratory diagnostics as well as clinical IT. In fiscal 2016, which ended on September 30, 2016, Siemens generated revenue of €79.6 billion and net income of €5.6 billion. At the end of September 2016, the company had around 351,000 employees worldwide. Further information is available on the Internet at www.siemens.com.
Read more

Contact

Dietrich Biester

Siemens AG

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 7-33559

Sabrina Martin

Siemens AG

Freyeslebenstr. 1
91058 Erlangen
Germany

+49 (9131) 7-37168