Skip to main content

Expert-based optimization agorithms

The PDN Optimizer uses a two stage process to determine the optimum strategy for populating capacitors in the design being analyzed:

  1. Expert-based synthesis uses 5 different strategies based on commonly used techniques to create and refine capacitor populations. This process runs quickly and produces results that can be used as-is or used as a "seed" for subsequent optimization.
  2. Domain-aware genetic optimization operates on the output of the first stage and uses a successive "generational" algorithm to improve design performance. This is not a generic optimization algorithm; it is tuned for decoupling capacitor optimization and produces better results, more quickly than a generic optimizer would.
Expert System (Synthesizer) shows StompPeaks strategy, Run control, capacitor table, and U100.DDR_1V2 Computed/Target graph.

PDN optimization results

HyperLynx SI/PI interface shows Advanced Decoupling Wizard and report table with name, margin, capacitor count and types.

The HyperLynx PDN Optimizer produces a hyperlinked, HTML report that lists all the different capacitor configurations analyzed, along with detailed performance, configuration and cost data for each. This allows designers to evaluate the tradeoffs between different potential solutions and pick the configuration that best meets their particular design goals.

On-Demand webinar

Getting it right - run SI and PI simulations accurately

There’s no point in running SI/PI simulations if the tools you’re using don’t have the accuracy, capacity and performance to do the job in a reasonable timeframe.

This recorded theater presentation shares some of the advanced technology that HyperLynx uses to produce accurate results.

HyperLynx PI PowerScope shows a multicolored visualization, right-side options, and a current-density notice for L8_GND3.

Resources