別のブラウザを使用してください

お客様が使用しているブラウザは完全にサポートされていないため、このサイトの正しい表示とユーザビリティが制限されています。

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

現在のブラウザで続ける

Electrification of road freight transport

Road freight transport powered by electricity: Siemens’ eHighway system combines the efficiency of the railroad with the flexibility of trucks into an innovative freight traffic solution that is efficient, economical, and environmentally friendly.

The system makes it possible to reduce the use of fossil fuels and truck operating costs, at the same time eliminating local emissions such as CO2 and nitrogen oxides.

LOREM IPSUM DOLOR SIT AMET
LOREM IPSUM

LOREM IPSUM

LOREM IPSUM DOLOR SIT AMET

LOREM IPSUM DOLOR SIT AMET, CONSECTETUR ADIPISCING ELIT, SED DO EIUSMOD TEMPOR INCIDIDUNT UT LABORE ET DOLORE MAGNA ALIQUA. UT ENIM AD MINIM VENIAM, QUIS NOSTRUD EXERCITATION ULLAMCO LABORIS NISI UT ALIQUIP EX EA COMMODO CONSEQUAT. DUIS AUTE IRURE DOLOR IN REPREHENDERIT IN VOLUPTATE VELIT ESSE CILLUM DOLORE EU FUGIAT NULLA PARIATUR. EXCEPTEUR SINT OCCAECAT CUPIDATAT NON PROIDENT, SUNT IN CULPA QUI OFFICIA DESERUNT MOLLIT ANIM ID EST LABORUM.

The concept for electrification of road freight traffic consists of three core elements: the energy supply, the pantograph, and hybrid drive technology.

Energy supply

The energy supply system is based on proven technology from the world of railroad electrification. The two-pole catenary system ensures a reliable energy supply for the eHighway truck. The catenary system leads to a level contact wire that enables stable current transmission, even at high speeds. The overhead contact lines are supplied with energy from substations equipped with:

  • Medium voltage switchgear
  • Power transformers
  • Rectifiers
  • Controlled inverters (for feedback of the electric energy generated by the vehicles’ regenerative braking)

Pantograph

The active pantograph transmits the energy from the overhead contact lines to the electric motor of the eHighway truck. The pantograph can be easily connected to and disconnected from the contact wire at speeds ranging from 0 to 90 km/h. This is done either automatically or manually at the push of a button.

Steering an eHighway truck connected to the overhead contact lines is no different to driving a diesel truck, as the active pantograph compensates for any shifts in position within the lane. The pantograph automatically disconnects in the event of evasive maneuvers or if the indicators are used.

Hybrid drive

On electrified routes, the electric motors in eHighway trucks are powered via the overhead contact lines and the active pantograph. For remaining sections of road, the eHighway truck has a hybrid drive. There are no restrictions on the type of hybrid drive: depending on the application and customer requirements, serial and parallel concepts with internal combustion engines, battery solutions, fuel cells etc. can all be implemented.

The electric motors of the eHighway trucks also enable recovery of the vehicle’s braking energy.

image

Heavily-used routes

Heavily-used truck routes, for example from ports to freight and distribution centers, are often a burden on the environment. In these situations, the eHighway system produces a significant reduction in pollutant and CO2 emissions. At the same time, the economic benefits of the system are felt particularly quickly on these high-use routes.

Mine transport

The eHighway is an ideal way to connect pits and mines with warehouses, transshipment points or processing plants. The economic benefits of the eHighway system can be easily calculated on the basis of transport volumes. At the same time, the eHighway system significantly reduces environmental pollution and dependence on fossil fuels.

Highways

Global road freight is forecasted to increase by nearly 400% over the coming four decades. This will bring with it a strong growth in CO2 emissions. In view of global goals to reduce CO2, it will be necessary to reduce road freight emission. Achieving this is a major challenge, especially when demand for road freight is increasing.

The eHighway system is based on a safe and proven infrastructure to provide a continuous energy supply to heavy commercial vehicles. It can be integrated and operated within the existing road infrastructure without significant effort and combines the efficiency of the railroad with the flexibility of trucks, halving energy consumption while maintaining full mobility. The eHighway system enables trucks to use renewable energy and can contribute significantly to reducing CO2 emissions. Both the ecological and economic advantages of the eHighway system grow with increased use of the route.

LOREM IPSUM

LOREM IPSUM DOLOR SIT AMET

LOREM IPSUM DOLOR SIT AMET, CONSECTETUR ADIPISCING ELIT, SED DO EIUSMOD TEMPOR INCIDIDUNT UT LABORE ET DOLORE MAGNA ALIQUA. UT ENIM AD MINIM VENIAM, QUIS NOSTRUD EXERCITATION ULLAMCO LABORIS NISI UT ALIQUIP EX EA COMMODO CONSEQUAT. DUIS AUTE IRURE DOLOR IN REPREHENDERIT IN VOLUPTATE VELIT ESSE CILLUM DOLORE EU FUGIAT NULLA PARIATUR. EXCEPTEUR SINT OCCAECAT CUPIDATAT NON PROIDENT, SUNT IN CULPA QUI OFFICIA DESERUNT MOLLIT ANIM ID EST LABORUM.

LOREM IPSUM

LOREM IPSUM DOLOR SIT AMET

LOREM IPSUM DOLOR SIT AMET, CONSECTETUR ADIPISCING ELIT, SED DO EIUSMOD TEMPOR INCIDIDUNT UT LABORE ET DOLORE MAGNA ALIQUA. UT ENIM AD MINIM VENIAM, QUIS NOSTRUD EXERCITATION ULLAMCO LABORIS NISI UT ALIQUIP EX EA COMMODO CONSEQUAT. DUIS AUTE IRURE DOLOR IN REPREHENDERIT IN VOLUPTATE VELIT ESSE CILLUM DOLORE EU FUGIAT NULLA PARIATUR. EXCEPTEUR SINT OCCAECAT CUPIDATAT NON PROIDENT, SUNT IN CULPA QUI OFFICIA DESERUNT MOLLIT ANIM ID EST LABORUM.

Our experts will answer your questions.
Please contact us