Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Mit dem aktuellen Browser fortfahren

Modern G1 for the U1 line

21 four-car metro trains for Nuremberg, Germany

New type G1 trains will modernize the U1 line – the oldest and longest of the three underground lines in Nuremberg.

Modern trains for Nuremberg’s oldest metro line

The metro line U1 is the oldest and longest of Nuremberg’s three underground lines and also has the highest number of passengers. It runs from the Nuremberg neighborhood of Langwasser via the Exhibition Center and Nuremberg Main Station to the neighboring city of Fürth.

With a total distance of 18.5 kilometers and 27 stations (out of a total of 48 stations in the Nuremberg/Fürth metropolitan area), on weekdays numerous commuters and students in particular use the U1 line. The number of passengers increases dramatically when there are major events, such as the Nuremberg Christmas Market and trade fairs. 

 

For increased passenger comfort and an optimized passenger flow, in November 2015 Nuremberg’s mass transit operator VAG Verkehrs-Aktiengesellschaft Nuremberg awarded an order to Siemens AG to supply 21 four-car G1-type trains. This rolling stock will replace 42 old DT1-type two-car trainsets. The order includes two options for an additional 13 trains.

Metro trains for Nuremberg

Fast and comfortable travel to the Nuremberg Exhibition Center and the Christmas Market with the G1

The new type G1 trains for Metro Nuremberg offer wider passenger doors with innovative LED light signals. Combined with an unobstructed passageway throughout the four-car trains, these features improve the passenger flow. In addition, automatic sliding steps at all the doors ensure optimal barrier-free boarding and exiting.

 

The bright and friendly design of the entire interior area with its generous multifunction areas creates a subjective sense of safety and guarantees a pleasant ride. For the drivers, too, attention was paid to ensuring a high level of workplace comfort: The driver’s cabin is set up to enable the driver to operate the train either standing or sitting.

 

The four-car trains are expected to enter into service starting in the fall of 2018.

Nuremberg metro train highlights

  • Greater passenger comfort – thanks to generous multifunction areas and air conditioning for the passenger area
  • Optimal work ergonomics – ergonomic workplace for drivers while standing or sitting
  • Greater passenger safety and accessibility – thanks to automatic sliding steps on all doors
  • Low energy consumption – thanks to the lightweight aluminum design, storage heating, and LED lighting
  • Improved passenger flow – thanks to wider doors with innovative LED indication strips
More about our metro trains:
Metro trains from Siemens