Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Ventotene – an off-the-grid Italian island

A modern power supply for a remote island in the Mediterranean

The Italian energy utility Enel Produzione SPA had a clear goal for the island of Ventotene: a stable power supply system that would operate more sustainably, economically, and reliably. And Siemens had the complete solution: The SIESTORAGE storage system, optimally combined with the Microgrid Controller.

A small island with a major challenge

The island of Ventotene was not connected to the Italian power grid. The existing supply system consisted of four diesel generators at 600 kWh each and a photovoltaic system. It was important that the power supply system keep pace with the small Mediterranean island’s growing economy.

image

The design of the entire network had to be made more efficient, ecological, and stable – using intelligent, innovative solutions.

This approach included the integration of renewable energy sources to reduce the supply of diesel and to create greater sustainability. An additional goal was to perfectly coordinate all existing and new power components and, even more important, to respond quickly and reliably to grid fluctuations, ultimately guaranteeing a stable network.

A modern, progressive island

The island of Ventotene is located in the Mediterranean about 100 km from Rome. Around 700 people occupy an area of 153 hectares – until the summer months, when the number of inhabitants grows to more than 3,000. It’s an extreme situation, including for the power supply system.

image

The Italian energy utility Enel Produzione SPA brought these requirements to Siemens. The challenge was to develop a complete, customized solution for supplying power to Ventotene. The focus was on a consistently reliable and stable system – a system that would also increase the efficiency of the existing diesel generators while making maximum use of renewable energies – and working with a qualified partner that could offer everything from a single source.

image

We were interested not only in pricing but in competence, reliability, and sustainability. And we were looking for a partner who shared our values.

ENEL, Italy
Project flyer
Download

A customized solution for a state-of-the-art g