Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser


In the past, Stedin has experienced power failures in its distribution grid. In addition to displeased customers, those events entailed expensive compensation payments for Stedin. Reliable energy distribution has always been Stedin’s core task, and so their main objective is to significantly reduce the SAIDI (system average interruption duration index) in their medium-voltage grids.


Today there are several self-healing distribution grids in operation worldwide, but they are usually built for overhead distribution feeders, primarily by applying automatic reclosers. The Dutch MV distribution grid, however, consists of underground cables, which cannot be quickly repaired in the event of faults, nor can they be fixed with automatic reclosers. Therefore a solution had to be developed that would work for the Dutch network system.

Rheinische NETZGesellschaft mbH
Local control unit for self-healing grid

The self-healing algorithm is elegant, simple, and robust and works for almost all grid structures. The applied RTUs and the developed software are very stable.

Dr. E. J. Coster, Expert Asset Manager Stedin


In collaboration with Stedin, Siemens developed a self-healing network solution. Substation automation was upgraded by implementing new distribution grid automation functions. The solution, which is based on a “regional controller” on the level of the substation, ensures automatic fault localization, isolation and restoration. The regional controller serves as an interface to the control center, which collects data from the distribution grid and hosts the regional, centralized applications of Stedin’s self-healing grid.


Part of the solution consists of an intelligent local substation. Upgrade kits were installed to modernize older ring main units (RMUs), or where that was not possible, older RMUs were replaced with new RMUs.


With the innovative self-healing grid solution installed, Stedin will significantly reduce its SAIDI and re-supply most of its customers with power in less than a minute in the event of a power outage.


This will result in both satisfied customers as well as considerable cost savings by minimizing the heavy contractual penalties that must be paid in case of power outages.

Rheinische NETZGesellschaft mbH
System configuration of a self-healing grid with a regional controller