Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Benson® technology

image

Highly efficient, flexible and reliable technology for steam generation

Benson technology is a proven process for large-scale steam generation in power plants. The heart of this process is the once-through principle. Combined with sliding pressure operation, this allows for highly efficient, flexible, and reliable power plant operation.

Our Benson technology and our associated Benson license will improve your specific steam generator and, consequently, benefit your power plant performance. Find out more below or contact us.

Benson technology

Experience and expertise

Since 1933 leading steam generator manufacturers have constructed Benson steam generators worldwide under Siemens Benson license. Today, our Benson technology is widely used in fired steam generators and heat recovery steam generators of highly efficient modern power plants.

For more information please click on the link below

Superior technology for the latest power plant applications

Today combined cycle gas power plants need to be more efficient and flexible than ever, because they have to both

  • Cover peak loads and
  • Serve as backup reserves for renewables

This is where Benson HRSGs make an important contribution. The unique once-through design enables fast flexible start up of a combined cycle, while maintaining high cycle efficiency. Benson HRSGs can be constructed either horizontally or vertically and will fit into any power plant architecture.

 

 

Benefits compared with drum-type steam generators

  • Steam parameters can be increased because there is no pressure limitation
  • Increased efficiency in part-load operation and at high ambient temperatures, thanks to reduced attemperator flows compared with a drum-type HRSG
  • Increasing operational flexibility: no limit on gas turbine load transients during startup and load changes, and no limit on load transients for possible duct firing

The first combined cycle power plant with a Benson heat-recovery steam generator (HRSG) – the 390-MW Cottam CDC, located in Great Britain – was successfully commissioned in 1999. More than 100 Benson heat-recovery steam generators have been commissioned to date or are currently under construction.

 

DrumType vs Benson Steam Generator

Supercritical pressure for maximum efficiency

The overall efficiency of a steam power plant counts in every respect, whether it’s reducing emissions or increasing economic efficiency. The best way to boost efficiency is by selecting high steam parameters. The once-through principle permits steam generation even at supercritical pressure. To date Benson boilers have been built for pressures up to 310 bar.

 

Contribution to flexible power plant operation

The Benson steam generator is especially well suited to flexible sliding-pressure operation: A steam power plant with a Benson steam generator can sustain load transients of four to six percent per minute over a wide power output range. High plant efficiency is ensured even at part load.

 

Sophisticated construction ­– individually optimized

Benson steam generators can be precisely adapted to suit your firing conditions: Different furnace sizes and geometries can be used depending on the fuel used. An important factor here is that the functions on the water/steam side are not restricted. Benson steam generators have been constructed with the broadest possible range of firing systems, including fluidized bed combustion.

 

Lately, the Benson steam generator with vertical rifled tubes has been successfully established in the market. Based on the Benson Low Mass Flux Design, this type of steam generator combines outstanding operating characteristics with low investment costs and high levels of reliability.

 

More than 1,300 Benson fired steam generators have been commissioned to date.

Test Rig

Start with something good – and make it even better

Benson steam generators have outstanding operating characteristics and are extremely reliable – thanks to continuous research and development. And we are refining the technology even more: We’re working intensively to optimize the heat transfer, pressure drop, and flow stability of two phase flows in evaporator tubes. Siemens has its own Benson test rig for the trials. The results of the trials have led to the creation of the world’s largest database on heat transfer and pressure drop in evaporator tubes, and support the development and validation of the Siemens Benson design software.

 

Another key area of focus is the development of Benson-specific control concepts, which make a key contribution to ensuring the best possible operation of your particular system.

License and services by Siemens

A profound package

The Siemens Benson license is available for fired steam generators as well as for heat-recovery steam generators. It primarily addresses the thermodynamic and thermo-hydraulic design of the evaporator system in Benson steam generators. 

Basically, the license comprises the following components:

 

-       Use of Siemens patents for the construction of Benson steam generators

-       Use of specifically developed and highly specialized Benson design software

-       Training and consulting

-       Transfer of the latest findings from research and development

 

In addition to providing the Benson license, we also advise utilities on questions related to the evaporator system of once-through steam generators.

 

Download references of fired Benson steam generators

Download references of Benson HRSGs

Download list of Benson licensees

 

 

Downloads and support

Your source of information

This is where you can find contact details and downloads to the services we offer.

References of fired Benson steam generators

References of Benson HRSGs

List of Benson licensees

Article - Benson low mass flux evaporators

Flyer Benson HRSGs

Flyer Fired Benson steam generators

Flyer Benson test rig

Support

Siemens AG
Freyeslebenstrasse 1
91058 Erlangen

(Charges depending on provider)
(From the German fixed network € 0.14/min.
and from the German mobile phone networks max. € 0.42/min.)

A selection of our projects around the world

image
image
image
image
image
image

Give your steam generator a boost

Benson technology will make the difference:  and we’ll find the right solution for your needs.

 

Talk to us about your particular challenge
Contact