Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Creating perfect places

A perfect place is a place that’s perfect for a purpose

At Switzerland’s Feldschlösschen brewery, the words ‘since 1876’ appear on every bottle. That’s not just a statement. It’s a philosophy. The same brewing methods since 1876. The same recipes. The same quality. A promise that every beer will be as good as the last. And if the brewery is protected, their product is protected – and their tradition is protected. Fire safety systems from Siemens protect Feldschlösschen’s most important ingredient: The building.

A perfect place to keep a tradition on tap

Feldschlösschen: The building is the beer

Feldschlösschen translates into "Little castle in the field". A poetic name for a special place. Feldschlösschen is not just an average production facility, but a place that breathes craftsmanship and tradition. It is also the name of the beer, printed of every single label for 140 years. Since then, every beer has been as good as the last.

image

Feldschlösschen beer without its tradition, without the building, that’s impossible.

Bruno Born, master brewer at Feldschlösschen brewery

brewery varieties of beer 16 1876 1877 1878 1879 1880 1881 1882 1883 1884 1885 1886 1896 1906 1936 1956 1976 1996 2000 2010 2011 2012 2013 2014 2015 2016 2017 Over years of tradition 141 employees 1,200