Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Ready for anything

OptimaFlex is a radically different direct drive approach that combines advanced site design with bespoke product solutions to offer variable rating wind turbines that are right for you and only you. It doesn’t stop there. Each wind turbine can be finely tuned throughout its lifetime to respond to changing conditions – be they climatic, topographical, or even economic. With a reduction of Levelized Cost of Energy (LCoE) of up to 15% per project, OptimaFlex gives you the optimal wind turbine configuration and project layout on day one and for every single day thereafter.

Unparalleled flexibility at every stage of your project’s life cycle

We engage with you at the first opportunity to develop a high-definition view of every detail of your project. Both our sales team and full contingent of engineers work with you to gain an appreciation of the geographical and climatic conditions at your site, as well as the priorities of your business. Only such an in-depth collaboration gives you confidence that the approach taken will deliver maximum profitability and returns over your project’s lifetime.

 

We first make a thorough analysis of the topography and conditions at your site. And after a process of comprehensive consultation with your business, we use CFD modelling and load analysis to make proposals for turbine selection and configuration as well as BoP layout that will maximize returns for your project over its lifetime. Early collaboration with our customers also allows us to make preliminary grid studies to ensure grid performance optimization from day one and into the future.

 

Our design and engineering teams will also take into account the business case for your project to make sure the layout and site design solutions we bring you will deliver against your commercial objectives.

A flexible product platform

Our product portfolio represents a fresh approach to wind power. Conventionally, turbines are designed to meet the demands of the most challenging conditions: the most remote sites, severe legal restrictions, extreme ambient temperatures and so on. While this results in products that more or less fit all sites, they will be sub-optimally designed for some if not all. OptimaFlex is a radical departure from this off-the-peg philosophy. The deep insights we gain through collaboration with our customers are transformed into bespoke solutions – solutions that fit your needs precisely.

image
image

Putting analysis into practice – delivering precisely the right product configuration for you

OptimaFlex represents an entirely new way to buy wind turbines. Its inherent flexibility, derived from the combination of our direct drive technology with the SICS control system and full-scale converter, allows you to select exactly the right turbine setup for your needs.

 

We take the learnings collected in the design phase and make precise calculations to work out exactly the rotor size, nameplate rating, and tower solution that will deliver the optimum returns for your project.

 

This market-leading level of flexibility is offered on a robust product that you can trust. Our direct drive offering has been at the forefront of gearless turbine design for 10 years, and our product design approach means turbine components and nacelle designs are standardized and modular across the range.

 

OptimaFlex - Reduced noise mode for wind turbines

Noise modes to put you in control of local noise emission regulations compliance

Through our unique software tuning, the turbine can be programmed to operate on a scale of noise modes. These noise modes allow for an optimal trade-off to be reached between maximization of output and compliance with noise regulations. These modes are responsive to any or all of the following parameters: sound power level, day of the week, time of day, wind direction or wind speed.

Flexible tower design: moving from off-the-peg to tailor-made

Traditionally, wind turbine towers are made to withstand extreme wind. However, our innovative flexible tower design approach delivers tower designs that are built with the precise needs of your project in mind. Height, steel shell thickness, materials and bottom flange diameters can be precisely optimized for your project. The result is a tower that is not overengineered, but just right for your needs. We have proven experience in producing site-specific tower solutions – experience that OptimaFlex builds upon. Significant investment in our processes and infrastructure allows us to deliver new levels of customization. This flexible tower concept is another example of how close collaboration between our engineers and our customers can pay dividends for years to come. By completely understanding the fine detail of your project and listening to your issues, we can build the perfect solution for your site and business plan.

Ongoing Optimization

OptimaFlex is ready for anything, meaning our turbines will be able to react to contingencies as they arise over the lifetime of your project.