Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

The road to a sustainable bio economy

Get ready for a sustainable and efficient future with new markets, materials, and applications

Innovative automation and digitalization solutions from Siemens ensure sustainability and efficiency in the fiber industry and beyond. With our in-depth knowledge of trends, we're your partner with an eye on the future.

New business opportunities

Explore new materials and new markets

In order to preserve our natural resources, it's essential that we use them as efficiently as possible. Opening up new markets and finding many new sustainable materials is an important part of our effort to use our resources with the utmost efficiency.

Finding new paths through the jungle of materials

When we think of using natural resources for products and applications, we often imagine a commonly used material: wood. But what if you could save money, go easy on the environment, and increase the value and yield of wood as a raw material for a broad variety of both "old-fashioned" and new products? There are a lot materials that might serve as our main fiber resources in the future. Think of plants like grasses, straw, banana peels, and eucalyptus, all of which are fast-growing and natural raw materials from which cellulose can be obtained thanks to new technologies.

Or how about producing items like clothes, compounds, insulating and composite materials, papers, and packaging using former waste products like hops extract residues, pomace, tomato stalks, or nutshells? That's not far-fetched: For example, the Netherlands alone produces a wet mass of 70,000 tons of tomato stalks each year. These stalks can already be introduced, inter alia, into solid board packaging. Using new materials like biogenic waste materials and by-products from other industries doesn't just pay off financially and environmentally, it can also deliver new properties like greater stability or a special feel for paper, tissue, and board products.

And the future holds even more possibilities – from highly profitable biorefineries to bio-based chemicals and consumer products.

Wood

As one of the best known and commonly used materials, wood is the epitome of a renewable raw material.

Grass

With its fast growth and extreme robustness, grass could be the raw material of the future. It can be harvested locally several times per year and has unique strength properties.

Eucalyptus

Eucalyptus is an excellent alternative to other raw materials: It is fast growing and there's no watering or use of pesticides necessary.

Tomatoes/Nut shells

As food industry waste products tomatoe stalks/ nut shells qualify as outstanding alternatives to other materials that have to be grown specifically for industrial use.

New applications

Explore new materials and new markets

Fiber products are conquering more and more industrial and consumer fields – and not just for environmental reasons. In the food and beverage industry, for example, sustainable materials can replace plastic wrapping, increasing food safety with improved properties for food preservation. In the textile industry, replacing cotton with fiber products opens up more acreage for food crops. The automotive industry has started using plant fibers for manufacturing lightweight car bodies. And there's more to come.

image

Biochemicals for the cosmetics industry

Natural and plant-based ingredients have been used for skin care for centuries. The market for natural cosmetics is growing. And when it comes to cosmetics in general, an increasing number of consumers are concerned about synthetic and chemical ingredients. That’s why the chemical industry is looking for new natural, eco-friendly raw materials with characteristics like binding, viscosity-increasing, texturizing, and peeling. Among the promising organic and sustainable ingredients for creams, shampoos, facial masks, toothpastes, deodorants, exfoliating shower gels, and many more cosmetic applications are substances extracted from eucalyptus as well as cellulose fibers from bamboo, grains, and other plants.

image

Biofuel for a green boost in your tank

Environmental issues and the limited availability of fossil fuel make it necessary to look for alternatives. Biofuels are made from biomass and are therefore renewable. They're also considered to be CO2 neutral, because they emit CO2 in the same amount that the living plants removed from the atmosphere via photosynthesis. Bioethanol is one the world's leading solutions. To defuse the ethical conflict of “food or fuel” – in terms of competition for acreage – experts are trying to figure out how to use only the parts of plants for the production of fuel that aren't edible, and how to fraction cellulose fibers. Using waste products from pulp and paper production like black liquor and fiber mud will also contribute to the future of biofuel manufacturing.

image

Ecofriendly construction with insulation materials

Whether it's due to new ecological construction concepts, regulations, and certifications, health issues, or the environmental impact of product manufacture, use, and disposal – the construction industry is increasingly relying on environmentally-friendly filling and insulating materials made of pulp or fibers. The insulation performance of natural insulating materials is equivalent to that of mineral and  synthetic insulating materials. But the natural insulating materials are less risky for the installer than, for example, fiberglass, and it's harmless and easy to handle for disposal. And there's more: Specialists are already working on papers that can be used to reinforce house components that are subject to especially high loads.
 

Learn more about the research project “Building with paper”

Siemens solutions

Get ready for innovations with a strong partner

Backed by more than 100 years of expertise and experience in the pulp and paper industry, Siemens accompanies this industry's transition to the fiber business and takes it even further, to new applications and markets. We provide indispensable support to the fiber industry with a comprehensive portfolio and long-term partnerships.

Our innovative solutions for the fiber industry