Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Intelligent Infrastructure

Speed Opens New Opportunities

In this day and age you can live in Tver and work in Moscow or nearby cities. In today's world people are ready to cover long distances in search of new opportunities. Thanks to the Lastochka commuter trains produced by Siemens for Russian Railways, passengers can now reach their destinations quicker and with more comfort.

image

The Lastochka train is adapted to Russian conditions, which means not only resistance to air temperatures as low as -40 °C but also compatibility of the car body and bogies to the 1520 mm-wide gauge. Large multifunctional zones in the passenger cabin provide enough space for oversize luggage, there are dedicated seats for people with limited physical abilities, and the cabins are fitted with climate control equipment ensuring comfortable temperatures throughout the trip. A passive safety system protects passengers and the crew in the unlikely event of an accident. 

 

Lastochkas run as fast as 160 kilometres per hour. Lightweight car design and pneumatic suspension ensure high comfort at any speed. 

 

The first Desiro RUS (Lastochka) trains were ordered by Russian Railways in 2009 and produced at our own plant in Germany. In 2011, OJSC Russian Railways placed an order for 1200 more Lastochka cars. The production of these cars has been localized near Yekaterinburg at Ural Locomotives, a joint venture of Siemens and the SINARA Group. By 2017 Siemens will achieve 80% localization of the Lastochka train production in Russia.

 

Siemens also provides maintenance services for the whole Lastochka fleet. Throughout a 40-years timespan they will be serviced at motive power depots in Moscow and Adler. 

 

Passenger operation of the electric trains started in 2013. In early 2014, they were carrying the athletes and spectators to the various locations of the Sochi Winter Olympics.

 

The first line where locally produced Lastochkas were introduced was the Moscow – Tver route. Thanks to the introduction of these trains, travel time between the two cities was reduced by half. Now passengers can reach Moscow from Tver in only one hour and a half. 

 

Today, Lastochkas already connect cities in six regions of Russia, ensuring the comfort and safety of thousands of passengers. In the future these trains will be used as rolling stock at the Moscow Railway Small Ring which is planned to start operating in 2016.

Infographic

Lastochka

Lastochka trains connect Russian cities, providing speed, comfort and safety to thousands of passengers. These innovative trains produced by Siemens are adapted to Russian weather conditions. They are made in Russia and for Russia.

lastochkalastochka
80% - Localization

Lastochka trains will be almost entirely Russian by 2017.

160 kph – Max speed

Thanks to fast and comfortable railway transportation, more and more passengers choose the train over other means of transportation.

30% - Energy saving

Lastochka consumes around 30% less energy than other commuter trains that are now used in Russia.

1520 mm – Gauge of railway

Lastochka trains are adapted to run on Russian railways.

-40 to +40 °C

Lastochka trains are adapted to Russian weather conditions and can withstand extreme temperatures.

6 Regions

Lastochka trains run throughout Russia.

Review

Lastochka Commuter Train

Based on the Desiro platform, the Lastochka is a modern electric train with an advanced safety system and special body equipment. It is adapted to Russian conditions and ensures high passenger comfort and safety at any speed. Desiro is one of Siemens most successful commuter train platforms.

Made for Russia

The Lastochka train is adapted to Russian conditions, which means not only resistance to air temperatures as low as -40 °C but also compatibility of the car body and bogies to the 1520 mm-wide gauge. Large multifunctional zones in the passenger cabin provide enough space for oversize luggage, there are dedicated seats for people with limited physical abilities, and the cabins are fitted with climate control equipment ensuring comfortable temperatures throughout the trip.

High-Speed Lastochka

Lastochkas run as fast as 160 kilometres per hour. Lightweight car design and pneumatic suspension ensure high comfort at any speed. The first line where locally produced Lastochkas were introduced was the Moscow – Tver route. Thanks to the introduction of these commuter trains, travel time between the two cities was reduced by half. Now passengers can reach Moscow from Tver in only one hour and a half.

Safety Above All

The Lastochkas's passive safety system protects passengers and the crew in the unlikely event of an accident. Timely maintenance of the trains in state-of-the-art depots ensures reliable railway traffic between the cities. Throughout a 40-years timespan Siemens will be providing maintenance services for the whole fleet of Lastochkas.