Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Move containers as if by magic

Using invisible networks

Powerful industrial communication networks ensure uninterrupted data transfers around the clock, even in difficult environments. Used in conjunction with driverless transport systems, they provide for best results in terms of reliability and speed.

image

Wireless communication

Networks for which no challenge is too great

More than 80 percent of global materials transport takes place by sea, with about 70 percent in containers – and this share is rising. Reliable wireless communication networks make this huge volume of traffic manageable. 

image

Reliable in wind and any weather

Average ship capacity has increased more than tenfold since the beginning of container transport, currently exceeding 8,000 TEU compared with about 700 TEU in the 1960s. Even capacities of over 13,000 TEU are not rare.

The resulting challenges for container terminals are enormous – and demand innovative solutions. Examples are warehouse blocks with gantry cranes, driverless transport vehicles, and automated container transport vehicles. These innovations, however, need to work together efficiently as part of an overall system to make full use of their potential. Industrial wireless networks play a key role: Even in extreme conditions, they ensure secure data communication in real time along the entire value chain – and also maximum reliability, efficiency, and availability at the container terminal.

Industrial WLAN

Wireless networks for industrial settings

There’s a lot in favor of WLAN in industry: significant cost savings thanks to lower wiring expense and clear benefits in flexibility and mobility. Wireless networks can also contribute to reducing energy and material consumption, cutting production costs, and improving productivity. But they also have to meet the special requirements imposed by the industry.

image

Expertise in design and implementation

How can industrial WLAN networks be designed right now for the demands of the future? At first glance, the process should be the same as for an office setting, but a closer look shows some differences – sometimes quite significant ones – that need to be considered, not just during implementation but ideally during the initial design stages. At an early stage, network experts should review the situation by taking measurements and checking the WLAN networks that may already be in place plus any new ones required, as well as potential new access points.

Design future-proof wireless networks
End-to-end WLAN infrastructures (pdf)

Partner of industry

Products and services for industrial networks

The planning, design, and implementation of reliable and powerful communication networks demand both ability and technical knowledge. We are your skilled partner in helping ensure that your company-wide communications are designed to be future-proof.