Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Siemens at SPS IPC Drives 2017

Discover the value of the Digital Enterprise.

SPS IPC Drives 2017, November 28 - 30, 2017

Hall 11, Nuremberg exhibition center

SPS IPC Drives

Discover the value of the Digital Enterprise.

We showed how our Digital Enterprise portfolio is offering scalable digital solutions that are helping companies to stay ahead of the competition and utilize the potential of digitalization.

We presented how digital twins provide major advantages for machine building and plant engineering. The MindSphere Lounge showed an immersive journey with our open IoT operating system. At our Thought Leaders Forum you were able to experience what opportunities you have to lead the future.

 

Write your own digitalization story.

Thought Leaders Forum and MindSphere Lounge

Presentations live, via livestream and for download

Impressions

Overview exhibition presence

Advancements. Innovations. Future.

Exhibits in details

Our innovations that you definitely should have a look at

Siemens has shown especially impressive solution for digital companies at SPS IPC Drives. Additionally, many more new products were presented.

image

SIMATIC S7-1500

The multifunctional platform on the basis of the S7-1500 offers the possibility to run high level language programs parallel to the user program without additional PC hardware.

SIMATIC S7-1500
image

SIMATIC S7-1500 system power supply

The system power supply PS 60W DC HF for retentivity reduces machine downtimes because at power down no data gets lost. All data of a SIMATIC S7-1500 CPU are saved thanks to energy buffering.

image

From integrated Engineering to Integrated operations

Interplay of all tools in one common data platform, every involved project discipline works on a common data basis.

Seamless and optimized data flow on all levels and over the whole lifecycle of the plant.

From integrated Engineering to Integrated operations
image

Know your motors better - with SIMOTICS IQ

With SIMOTICS IQ you get your motors under control, anytime and anywhere. Thanks to a cloud connection and data analysis, the motors are part of your digital enterprise. Benefits: Higher availability. Increased performance. Optimized serviceability.

SIMOTICS IQ
image

SINAMICS V20 I/O Extension Module

The SINAMICS V20 I/O Extension Module provides two additional digital inputs and two relay outputs for the converter. With this new option the SINAMICS V20 converter gains additional functionalities such as multi-pump control.

SINAMICS V20 I/O Extension Module

SINAMICS S120 Booksize Motor Modules type C/D (24/45/60 ampere)

SINAMICS S120 Booksize Motor Modules type C/D: reduced space requirement in the control cabinet thanks to new frame sizes (45A/60A) and new types (24A). Modules with 24A now also available as type C and D.

SINAMICS S120 Booksize Motor Modules type C/D (24/45/60 ampere)
image

SINAMICS G120

Three additional push-through heat sink versions have been added to the PM240-2 Power Modules for the SINAMICS G120. With the new frame size FSG, the existing SINAMICS G120 range is extended up to 250 kW.

SINAMICS G120
image

Servo drive system SINAMICS S210

The simple, high-performance and safe SINAMICS S210 inverter forms a perfectly matched servo drive system together with a SIMOTICS S-1FK2 motor and the optimized OCC connection technology.

Servo drive system SINAMICS S210
image

Synchronous-reluctance drive system

1. High energy saving, especially in the partial-load operation

2. High productivity and operational reliability 

3. Perfectly harmonized drive system with SINAMICS converters

Synchronous-reluctance drive system

Drive system with water cooling for one common circuit

With their standard cooling concept, SINAMICS S120 and SIMOTICS FD are perfectly matched. The quality requirements of the cooling water of the system are very low, which means the system can be cooled with water normally used in industries.

image

Digital Drive Train Services

With Digital Drive Train Services Siemens offers you not only the hardware, the connectivity and the platform, but also the related Digital Services – and this throughout the entire drive train.

Digital Drive Train Services
image

SIMOTICS SD Add

The new efficient  generation of low-voltage motors can now also be used in process industries, especially oil & gas, petrochemical and chemical. Via the SIMOTICS Digital Data App the most important motor data can be retrieved at any time. 

SIMOTICS SD next generation

Industrial Security for industrial networks

- Secured networks as indispensable part of a holistic security concept 

- Access violations prevented by a firewall

- Secured communication thanks to VPN tunnel and security engineering in the TIA Portal

Industrial Security for industrial networks
image

New IWLAN products for the industry and industry-oriented sectors

-Gigabit data rates thanks to IEEE 802.11ac Wave 2, for video streaming/ high-density

-Industrial software features such as iPRP for reliable IWLAN communication with redundancy over WLAN

-Rugged, compact devices, versatile mounting

New IWLAN products for the industry and industry-oriented sectors
image

Expertise in Industrial Networks – the basis for digitalization

-High data rates up to 10 Gbit/s and redundancy with SCALANCE X

-Industrial security with SCALANCE S/M

-iFeatures for stable communication in the radio field with SCALANCE W and Software for network management and secured remote access

Expertise in Industrial Networks

RUGGEDCOM RX1400 MindConnect

-Built-in MindConnect

-LTE (4G) Interface with Rollback to 2G/3G and integrated Wireless LAN Access Point/Client

-Full ROX2 solution suite and Virtual Machine Environment (RUGGEDCOM VPE1400)

RUGGEDCOM RX1400 with MindConnect
image

SIRIUS ACT with PROFINET

With the flexible communication solution SIRIUS ACT push buttons and signaling devices can be directly connected to the controller via PROFINET.

SIRIUS ACT with PROFINET
image

SIMOCODE pro goes MindSphere

When it comes to digitalization and the efforts to evaluate vast quantities of data rapidly, SIMOCODE pro transfers feeder data directly to the cloud via OPC UA. The result: greater plant availability and economy.

SIMOCODE pro goes MindSphere
image

Integrated Control Panels – Comprehensive support for control panel applications

When it comes to control panel planning, Siemens possesses knowledge, tools and data along with a coordinated product portfolio. The result: holistic support in managing the challenges involved in control panel engineering and building.

Integrated Control Panels – Comprehensive support for control panel applications
image

SIRIUS modular system – Efficiently combined

New: now with all sizes updated – mission accomplished

SIRIUS modular system offers everything you will need for switching, protecting, and starting motors and systems. Advantages for users:

SIRIUS modular system – Efficiently combined
image

SIMATIC MV540

With the SIMATIC MV540, the optical readers are expanded by a series of new high-end devices. The SIMATIC MV540 offers considerably greater functionality and performance, but is still fully compatible with the SIMATIC MV440 series.

SIMATIC MV540
image

SIMATIC RF380R

The new-generation SIMATIC RF380R reader has been significantly improved in its functionality, but remains fully compatible with the first generation. To achieve high reliability, especially in metallic environments, a new convenient setup assistant determines the optimal antenna position.

SIMATIC RF380R
image

SIMATIC RF280R

SIMATIC RF280R is a reader with integrated antenna for identification tasks in harsh industrial environments.

The Reader is particularly suitable for the use in dynamic applications and is mainly used in places where longer ranges are required.

SIMATIC RF280R
image

SIMATIC RF200 IO-Link V1.1

The new IO-Link reader series SIMATIC RF200 meets the IO-Link standard V1.1 and processes data more than ten times faster than readers with the IO-Link standard V1.0. The SIMATIC RF200 IO-Link readers represent the cost-efficient solution for simple identification tasks.

SIMATIC RF200 IO-Link V1.1
image

Digital Services Industry

Collect. Analyze. Realize. Profit.

Create added values through intelligent data collection and analysis – optimize your overall equipment effectiveness with Digital Services.

Digital Services Industry

Factory Automation Services

No Time for Downtime

We support manufacturers in their efforts to continuously optimize operation, carry out comprehesinve preventive maintenance and restore the functionality of their machines and plants as quickly as possible. 

Factory Automation Services
image

MindConnect

With MindConnect, Siemens offers numerous possibilities for connecting machines, plants and worldwide fleets to MindSphere, regardless of the manufacturer. e.g. MindConnect Nano

MindConnect
image

MindApps / 3rd party apps

MindApps open up new possibilities, allowing you to use your machine data to create added value.

MindApps / 3rd party apps
image

Power supply for Digitalization & Industry 4.0

The manufacturer-independent communication via OPC UA of the power supply system SITOP PSU8600 and the uninterruptible power supply SITOP UPS1600 allows energy management, diagnostics and preventive maintenance of 24 V DC load circuits.

Power supply for Digitalization & Industry 4.0
image

Smart, Clever. LOGO!Power (4th generation)

The innovative power supply devices designed into the LOGO!8 module offer great performance in the smallest space.

Smart, Clever. LOGO!Power (4th generation)
image

SIMATIC PCS 7 Plant Automation Accelerator – The next step towards the digital plant

With SIMATIC PCS 7 Plant Automation Accelerator our customers will benefit from a consistent engineering without any media breaks between automation engineering and the process control system

SIMATIC PCS 7 Plant Automation Accelerator
image

SIMIT 9.1 – Optimize your plant, increase your competitiveness

SIMIT simulation software permits real-time simulation and emulation for comprehensive examination of automation solutions. Either a real or virtual automation system is used for control (Virtual Controller). The connection to COMOS ensures a comprehensive data flow, creating the basis for the „Digital Twin“ of the plant. 

SIMIT 9.1
image

SIMATIC PCS 7 V.9.0 – Room for new perspectives

The new version V9.0 of our established and proven DCS SIMATIC PCS 7 provides you a significant plus of performance, based on more compact hardware and new software functions.

The result: Higher flexibility and efficiency.

SIMATIC PCS 7 V.9.0
image

SITRANS FS230

The digitally based SITRANS FS230 clamp-on ultrasonic flowmeter is a state-of-the-art, cost-effective flow measurement. Its high-performance transmitter features accuracy levels up to 0.5% and a best-in-class 100 Hz data update rate.

SITRANS FS230
image

SIRIUS Contactors S6-S12 with fail-safe control input

Siemens is extending its Sirius product portfolio to include new contactors in sizes S6 to S12. The new contactors for 55 kW and above have a certificated input for signals from pm-switching or pp-switching fail-safe or standard controls.

SIRIUS Contactors S6-S12 with fail-safe control input
image

New fail-safe digital output module for SIMATIC ET 200SP

New 8-channel F-DQ for ET 200SP

To safely control of solenoid valves, Contactors and non-isolated loads. Each output channel contains of 2 switches (pp-switching). Useable in applications up to SIL 3 and PL e

New fail-safe digital output module for SIMATIC ET 200SP
image

SIMATIC STEP7 Safety Advanced / Basic V15

New functions for usability and migration

Due to the new OV-Bit monitoring it is simpler to migrate existing programs of a S7-300 to S7-1500. The new F-signatures allow the faster identification of changes in the SW or HW. 

SIMATIC STEP7 Safety Advanced / Basic V15
image

Totally Integrated Automation

Automated execution of engineering tasks, PLM integration to automation engineering, efficient cloud based engineering, virtual commissioning, integrated energy management, machine and plant security, shorter time-to-market, increased flexibility, enhanced quality, increased efficiency, industrial security

Totally Integrated Automation
image

TIA Selection Tool

Ready for TIA Portal: the smart way to correct device selection and configuration for every automation project.

TIA Selection Tool
image

TIA Portal V15

TIA Portal V15 - News: multifunction platform with PLC 1518MFP, handling with S7-1500T technology PLC to realize 2D / 4D kinematics, S7-1500 supports OPC UA method calls

image

TIA Portal V15 - Virtual Commissioning

Interdisciplinary fields of work are increasingly becoming the focus: enables virtual validation, interaction between control components and the mechatronic system, reducing time and costs

image

Electrification goes MindSphere

Intelligent power distribution solutions provide data from the electric network for automated and efficient engineering. Applications based on open IoT ecosystems like MindSphere allow for an overarching data evaluation.

Electrification goes MindSphere
image

Power monitoring made simple

The power monitoring system from the SENTRON portfolio is optimally suited for small and medium-sized businesses. It enables an energy management system according to ISO 50001 and to permanently reduce energy costs in companies.

Power monitoring made simple
image

Intelligent Switchboard

The SIVACON S8 low-voltage switchboard is ready for the challenges of digitalization. The data of all connected devises are thus available for higher-level automation and energy management systems, or for cloud-based analysis systems.

Intelligent Switchboard
image

3VA molded case circuit breakers – portfolio expansion of breakers with a rated current till 1,000 A

As the core piece of power distribution systems, 3VA molded case circuit breakers ensure reliable, high-available production processes. They fulfill all basic requirements for networked and automated production environments. 

3VA molded case circuit breakers
image

“Discover the value of the Digital Enterprise” – in this year's slogan of the SPS IPC Drives fair from Siemens „value“ is one of the keywords and to create value financial freedom of action is needed. Siemens Financial Services offers all kind of financing opportunities.

Use the SPS IPC Drives fair to inform first-hand about innovative and future proofed financing models. Whether you are interested in digital twins, additive manufacturing or in general for automation and digitalization, whether you want to invest or to market your own solutions: our financing solutions offer you various possibilities.

 

The exclusive study from Siemens Financial Services helps you to find out which Productivity Bonus can be achieved by automating and digitalizing the production systems.

SPS IPC Drives info package

Stay tuned about news and information even after SPS IPC Drives fair – sign up now.