all
Miks Volumetric Machine Tool Compensation (VCS)?
Volumetric error measurement accounts for 21 errors in 3-axis systems, including positioning, straightness, pitch, yaw, roll, and squareness. AfM Technology can capture, evaluate, and correct these errors using modern tech. Installing a VCS file on the controller can improve accuracy up to 85% compared to "as found".
Eelised
- Up to 85% higher accuracy at the machine geometry
- Identification of mechanical vulnerabilities
- Tighter tolerances possible
Soovitatavad Võimalused
all
Analysis of the geometry
Tutvuge Ressursside ja Sellega Seotud Toodetega
Eeltingimused
VCS has to be installed on the controller