Skip to main content

Lincoln university

An intelligent campus starts with Intelligent Valves

A person is outside a brick-and-glass building with solar panels and a teal decorative entrance pattern.

Reference: A leading land-based sectors institution since 1878, aims for carbon neutrality by 2030 and a zero-carbon footprint by 2050.

Location: Lincoln, New Zealand.

Project Focus: a comprehensive building automation system with intelligent valves for enhanced energy efficiency and sustainability.

Championing sustainability

Lincoln University is a top land-based sectors university and has been tackling pressing environmental issues since 1878. It has set its own environmental targets of achieving carbon neutrality by 2030 and a zero-carbon footprint by 2050. To help meet these targets, the new research facilities needed a smart solution that would guarantee sustainable operations, as well as consistently identifying energy savings opportunities and measuring energy use for sustainability reporting.

Setpoint Solutions, a certified Siemens Building Automation Partner for over 20 years, has expertise in system integration and green building projects making them – together with Siemens’ innovative solutions – the perfect partner for this project.

It’s an honor for Siemens to work with Setpoint Solutions. They are consistent early adopters of our new technologies and are always willing participants in new product field tests and feedback sessions."
Paul McMullen, Regional Sales Manager, Siemens Building Products, New Zealand
ONE - lincoln-university

Realizing the vision with Intelligent Valves

To achieve the university’s energy efficiency goals, Siemens and Setpoint Solutions offered a building automation solution that includes building automation, building management, room automation, and lighting controls. The Building Management System (BMS) uses Siemens PXC automation controllers and TX I/O modules to manage inputs and control outputs. The solution also employs an extensive suite of Siemens Building Products including sensors, damper motors, control valves, and actuators for seamless operation.The key innovation of this project is found in the dynamic hydronic balancing solution. Setpoint Solutions deployed twenty Siemens EVG Intelligent Valves to control the primary air handling units across the new buildings. These valves are more than just system components, they are the keystones to operational efficiency and sustainability.

The project was initially specified and designed with standard motorized control valves; however, Setpoint Solutions’ engineers identified a significant opportunity for energy savings by upgrading to Siemens Intelligent Valves. As well as energy savings, the data gathered from the valves assists with remote maintenance and servicing.
Sam Hazlett, Director at Setpoint Solutions,

The ultimate sustainable solution for heating and cooling systems

infographic for real time tracking with person in front of screens

Real-time tracking for improved energy efficiency

The Siemens Intelligent Valve tracks flow rates, temperature and energy in real time, making energy calculation data transparent. Dynamic hydronic balancing automatically compensates for pressure fluctuations to avoid temperature variations in the research facilities and ensures room comfort for users as well as maximum energy efficiency.

Infographic for easy installation - hand and smartphone

Simple installation and streamlined operations

Installation and commissioning of the Intelligent Valves at the university was simple, intuitive, and quick, compared to standard valves, with only one short additional step for commissioning required. Additionally, the Siemens ABT Go app streamlines setup and adjustments with its user-friendly interface, making operations straightforward and efficient.

inforgraphic worker with yellow helmet in front of a visualized city

Reduced errors and improved reliability

In the university’s new buildings, the Intelligent Valves are set in their flow control mode which introduces further benefits during operation such as limiting the risk of human error; it also makes it easier to deal with alarms and identify problems at their root cause. Additional data from each Intelligent Valve provides service technicians with information to help with remote maintenance and servicing.

infographic for lower material costs

Lower material and energy costs

Material costs for Setpoint Solutions were lower due to fewer valves being needed in the system thanks to the Intelligent Valves' built-in flow limit capabilities. Lower materials costs coupled with higher energy savings will bring long-term costs savings to the university.

The installation and commissioning of Siemens' Intelligent Valves were simple, intuitive, and surprisingly fast.
André Kraenzlin,, Senior Systems Engineer, Setpoint
Picture of two women talking i a meeting room.

Tackling tomorrow’s challenges with today’s solutions

Investing in intelligent valves and smart building technologies will help Lincoln University cut energy use and improve operational efficiency in its new research facilities. This will bolster the university’s dedication to academic distinction by providing a sustainable campus infrastructure and an optimal learning environment for its students.Like many institutions, Lincoln University is modernizing outdated infrastructure and introducing flexibility to prepare for digital advancements. Intelligent Valves are smart devices that can be connected to the cloud via Siemens’ digital applications as part of our Building X suite. This offers additional benefits such as remote access to multiple sites, real-time visibility and operation, data trending and analysis, all with Siemens’ highly secure connection. Intelligent Valves have multiple protocols and are ready for system upgrades and future digitalization if the university elects to further digitalize their building management.

Begin your smart campus journey today

Siemens’ partnership with Setpoint Solutions and Lincoln University illustrates the power of smart building technologies and our collective environmental commitment. The university's journey inspires academic institutions worldwide to consider how digital transformation can create a smarter, more sustainable campus environment.

Inspired by the story and ready to embark on your smart campus transformation? Connect with us today to find out how we can support your efficiency and sustainability goals with eco-conscious innovation on your campus.

Picture of Lincoln University

Related references

Balancing IAQ and energy efficiency at Maine Township schools
Maine Township School District, Park Ridge, Research and education

  • A story about modernizing HVAC systems and controls in three large high schools.
  • HVAC system and controls installed 2,500 PICVs, 1,300 DXR2 controllers, 800 room unit sensors, 500 damper actuators, 100 variable frequency drives, 50 TC controllers and 10 PXCs.
  • The results: US$75,000 savings in first costs , 50% faster fresh air delivery , and 30% potential energy reduction from a more efficient hydronic system 
Image of Lincoln University

Shopping Mall Achieved Up to 25% Energy Savings with Siemens Intelligent Valve
Vega Subayevleri AVM, Ankara, Shopping Center

Siemens solution prevented approximately 25% inefficient energy consumption 

Siemens Intelligent Valves were chosen to manage energy consumption transparently and efficiently for more than 150 stores in the shopping center, and to reduce energy consumption at the same time.

Watch the video

Image of shopping mall in Ankara

Comfort tailored to each animal
Pairi Daiza, Belgium, Hospitaliy and entertainment

  • The comfort of animals and visitors is of paramount importance for Pairi Daiza. The climate must be perfect everywhere, both in the enclosures and in the hotels of the Pairi Daiza Resort.
  • Building technology from Siemens allows the temperature, humidity and air quality to be controlled perfectly without any discomfort for visitors.
  • Regardless of fluctuations in system demand, the installation adapts smoothly because it is equipped with automatically controlled Intelligent Valves from Siemens. This ensures optimal operation at any time.
Image of an white bear in a zoo - and a child standing in front of him