Skip to main content

Sistema de devolución

Siemens, s.r.o. se compromete con la responsabilidad medioambiental y coopera con ASEKOL y ECOBAT para garantizar el reciclaje ecológico de los residuos de aparatos eléctricos, baterías y acumuladores, y así conservar los recursos naturales y reducir los residuos de los vertederos.

Electrical equipment, batteries, and accumulators contain a large number of materials that have negative impacts on the environment and human health (e.g., lead, cadmium, or mercury). By handing over waste electrical equipment, batteries, and accumulators to collection points, we prevent the release of these harmful substances into the environment and at the same time enable their reuse.

Learn more about why it's important to recycle used electrical appliances here.

af6d9f1a-080c-4a4b-809e-e3a01afa2d6b - trash-recycle-illustration-bigstock-125163368-mhero-1280x720

Which electrical equipment, batteries, or accumulators should be recycled?

All waste electrical equipment, batteries, and accumulators are subject to recycling. These items are marked with a crossed-out wheeled bin symbol on the packaging, warranty card, or user manual. This symbol indicates that the equipment, batteries, or accumulators must not be disposed of in regular trash bins, containers, or municipal waste. If the crossed-out bin symbol is accompanied by a chemical symbol such as Hg, Cd, or Pb, it means the battery or accumulator contains more than 0.0005% mercury, 0.002% cadmium, or 0.004% lead by weight.

Disposing of such marked items in municipal waste containers or in nature is strictly prohibited.

¿Dónde se deben desechar los residuos de aparatos eléctricos, baterías o acumuladores?

Los residuos de aparatos eléctricos, baterías o acumuladores se pueden entregar de forma gratuita en todos los puntos de recogida de ASEKOL, que se encuentra en toda la República Checa. Puedes encontrar el punto de recogida (devolución) más cercano en www.asekol.cz/sberna-mista. Al entregar los residuos de aparatos eléctricos, baterías o acumuladores en un punto de recogida, te aseguras de que tenga un reciclaje ecológico.

Options for Disposing of Used Electrical Equipment

When delivering an order to the end user via a shipping service, you can take advantage of the option to dispose of used electrical equipment (one-for-one exchange). If you are interested in this service, please send your request along with the order number to: zpetnyodber.cz@siemens.com. This service is provided free of charge, based on invoicing and delivery of the same type of electrical equipment that the end user intends to return.

The collection of used electrical equipment can only be arranged if the service is requested within 14 days from the invoice date.

Recycling Fee

The recycling fee, i.e., the financial amount covering the ecological disposal of waste electrical equipment, is always included in the product price. The amount of this fee depends on the specific category of the electrical equipment and the pricing set by ASEKOL.

More Information

Detailed information about recycling can be found on the websites of ASEKOL and ECOBAT