Skip to main content
This page is displayed using automated translation. View in US English instead?

BACnet Gateway - People Counting to BMS control is powered by Terabee

People Counting Infrastructure - Enabling better use of space and energy

Our Mission - Towards ZERO emission buildings
We provide People Counting infrastructure to enable data analytics for Space, Energy and Operations Management, leading to Decarbonization, Energy and cost savings with fast Return-On-Investment (ROI).

Energy per person is the future metric - Today’s “Energy per square meter” reporting is not enough. An “energy-efficient” building that is under-utilized remains inefficient. Heating, cooling and ventilation expenses exist independently if allocated spaces are properly used.

Why Bridging People Counting Network with BMS?

Designed for BMS integrators and commercial building operators, the BACnet Gateway eliminates fragmented people counting data that restricts efficiency, security, and comfort. It connects Terabee sensors to any BMS via BACnet, providing real-time occupancy data on a centralized platform, with optional LoRa support. Value is measured by lower energy use, optimized HVAC & lighting control, improving space utilization across portfolios of any size.

Building management system diagram

Benefits

  • Bridging People Counting Network with BMS:
    The BACnet Gateway is connected to the Building Management System over IP and feeds relevant People Counting data. This makes the BMS smarter, enabling real-time building control based on the most important information: how the building is used by people.
  • Real-time control:
    When sensor data is collected for a control system, real-time is critically important. Both FLOW and OCCUPANCY People counters push data to the BACnet Gateway, which is capable of fusing data, translating & pushing relevant information to the BMS, all in real-time.
  • A powerful device management tool:
    The Gateway enables easy configuration of multiple People Counting devices at once, saving time and simplifying the commissioning process. It can also run firmware updates on the people counting devices connected to the gateway.
  • Space configuration and data fusion, locally:
    The Gateway host locally information about the building layout, including rooms and spaces. Both FLOW and OCCUPANCY People counters are assigned to specific areas so that aggregation and data fusion is performed on the Gateway.
  • 100% data integrity and security:
    Data integrity is ensured by the infrastructure being fully local, bringing total peace of mind for security concerns.

Featured Capabilities

Real-World Applications

Select...

Universities

Maximize efficiency of lecture halls, classrooms, areas based on actual usage patterns, energy and HVAC Management,
schedule custodial and maintenance staff according to real-time space occupancy, especially in high-traffic common areas and restrooms, class Scheduling & Course Planning