Direkt zum Hauptinhalt
Case Study

Optimal Control of Heat Generation and Distribution

The autonomous D-ACS system, developed at the Silesian University of Technology and based on Siemens PLC and EDGE technologies, optimizes heat generation and distribution, improving energy efficiency in the food and chemical industries.

The D-ACS (Development of an Autonomous Control System) project, conducted by the Faculty of Automatic Control, Electronics and Computer Science at the Silesian University of Technology, is developing an autonomous system for heat process control. The solution combines a PLC controller, a distributed ET200eco I/O system collecting sensor data via IO-Link, and an application running on the SIMATIC Industrial Edge platform or, optionally, in the cloud. The project is funded by the National Centre for Research and Development under the Lider XII programme.

Innovative Control System

It is estimated that more than 90% of control systems currently operating in the food and chemical industries do not perform optimally. In particular, they fail to provide the required level and quality of control for heat generation and distribution processes. This results in increased energy consumption, greater environmental impact, and excessive production downtime. The PID controller, the most commonly used industrial control solution, rarely delivers high performance due to improper tuning or an inefficient control structure.

“One way to improve the efficiency of industrial processes is through effective control of heat distribution and exchange systems, which are often key components of industrial installations,” emphasizes Michał Frątczak, PhD Eng., from the Silesian University of Technology.

Case Study - Silesian University of Technology 02 img

Up to 90% of control systems operating in the food and chemical industries may not perform optimally. Researchers at the Silesian University of Technology set out to change this.

Case Study - Silesian University of Technology 05 img

Advanced modeling and simulation methods for heat generation and distribution processes are employed throughout the project.

There is currently no sufficiently advanced, ready-to-use solution on the process automation market capable of diagnosing and effectively controlling heat distribution and exchange processes. The system being developed at the Silesian University of Technology has the potential to bridge the gap between scientific research and industrial needs.

“The scientific value of the project lies in the use of advanced modeling and simulation methods for heat generation and distribution processes. The research team’s innovative approach is based, among other things, on the application of a comprehensive physical model for the design and tuning of an advanced controller,” says Artur Nowocień, Application Support Expert at Siemens Poland.

Project Development Stages

The research project is being carried out using a heat distribution and exchange installation located in the technological laboratory of the Department of Automation and Robotics at the Faculty of Automatic Control, Electronics and Computer Science of the Silesian University of Technology. The laboratory setup includes an electric flow heater with modulated heating power and a configurable system of two plate heat exchangers. The facility is equipped with industrial temperature, pressure and flow sensors, as well as control valves that regulate liquid flow through the heater and both heat-exchanger circuits. This configuration enables the simulation of a thermal substation with a controllable heat source and a configurable set of heat consumers.

The project has been divided into five stages. The first involved developing a method for tuning process-model parameters and designing the IT application architecture. In the next stage, the research team developed a control algorithm together with an automatic retuning method, allowing adaptation to changing production conditions during operation. The researchers then designed a control system for an industrial flow heater and subsequently developed the dpB-BAC controller to regulate water flow in the primary circuit of a heat exchanger. Based on a process model and requiring dedicated tuning methods, the controller enables highly efficient system operation.

Case Study - Silesian University of Technology 05

For the research work and development of the D-ACS system, a heat distribution and exchange installation located in the technological laboratory of the Department of Automation and Robotics at the Faculty of Automatic Control, Electronics and Computer Science of the Silesian University of Technology was used.

Case Study - Silesian University of Technology 06

System D-ACS pracuje w oparciu o komputery EDGE Siemensa lub chmurę obliczeniową.

“In practice, the simplest trial-and-error approach is usually recommended, but it can be costly and does not always provide the required control performance. In our project, we developed an effective method for tuning the advanced dpB-BAC controller,”
explains Paweł Nowak, PhD Eng., from the Silesian University of Technology.

After developing the control algorithm and selecting the method for obtaining its settings, the dpB-BAC controller was transferred to a Siemens industrial PLC. For this purpose, a dedicated function block was programmed for Siemens S7-1200 and S7-1500 controllers. In addition to control functions, the block provides features such as switching between manual and automatic modes, manual setpoint adjustment, bumpless transfer, and output limiting. The completed dpB-BAC controller block was then integrated into the PLC program and connected to the application interface using previously developed and tested communication blocks.

The implemented software modules use communication mechanisms that support encryption, hashing, and tunneling algorithms. All of these features are aligned with the latest Industry 4.0 trends and the Industrial Internet of Things (IIoT).
Patryk Grelewicz, PhD Eng, Silesian University of Technology

The third stage of the project focused on evaluating control performance in heat generation and distribution systems. The outcome of this phase is an automatic control performance assessment system implemented as an application on the Industrial Edge platform and connected to a PLC controller. Based on measured process variables, the system provides operators with information about control quality.

“The system has been designed so that it can also be used in existing control installations with implemented algorithms such as PID controllers, significantly increasing the versatility and practical applicability of our solution,” explains Michał Frątczak, PhD Eng., from the Silesian University of Technology.

The fourth stage of the project, carried out in mid-2024, involved integrating the previously developed solutions and performing laboratory validation of the complete system. This phase employed a virtual commissioning approach. It enabled the consolidation of the methods developed during stages 1–3 through the implementation of the advanced controller function block and its integration with digital twins created in the SIMIT application. As a result, a unified autonomous control system was developed, based on a Siemens S7-1500 PLC and an Edge computer. Its operation was successfully validated using virtual commissioning techniques.

The final outcome of the research project will be verified during the last stage, scheduled for the fourth quarter of 2024, when the system will be tested under real industrial operating conditions.

Case Study - Silesian University of Technology 07

Siemens controllers are a key component of the system. D-ACS is compatible with solutions from the S7-1200 and S7-1500 product families.

In the final stage of the project, we plan to make the autonomous control system available to our industrial partners, including system integration companies, in order to evaluate its practical value and applicability for end customers
Paweł Nowak, PhD Eng., Silesian University of Technology

Flexible and Efficient Data Acquisition

The Siemens SIMATIC ET200eco distributed I/O modules with IP69K protection used in the project collect data from field sensors. Thanks to their ability to operate outside control cabinets, they can be installed directly next to sensors, reducing cabling requirements. Their enhanced resistance to harsh environmental conditions makes them particularly suitable for food and chemical industry applications, where the system is intended to operate. Support for the IO-Link protocol provides standardized connectivity with a wide range of field devices that may already be installed at customer sites.

The solution also incorporates the Field Data Enabler PN App, which can transparently read data from IO-Link devices without requiring modifications to the PLC program. This provides an alternative method of acquiring process data within the system.

“By using this approach, integration with a customer’s actual installation does not require interference with often highly complex and business-critical control programs, nor the need to obtain additional approvals from machine manufacturers, which can be difficult to secure. This concept provides a strong foundation and high flexibility for the system while ensuring stability and compliance with industrial application standards,” adds Mirosław Kuligowski, Sales Development Manager at Siemens.

Case Study - Silesian University of Technology 09

SIMATIC ET200eco modules collect data from field sensors. With their IP69K protection rating, they are well suited for use in industrial environments with demanding operating conditions.

The role of the edge platform

Case Study - Silesian University of Technology 10 img

The operation of the entire system was verified using digital twin technology.

The proposed solution is one of the few that combines industrial PLC controllers with the capabilities of an edge platform and cloud computing in such a comprehensive manner. The developed application can be deployed in both environments, enabling the control algorithm to run either entirely locally, directly at the installation site, or remotely, thereby increasing flexibility. The Edge computer collects and analyzes data, which is then used for model parameter estimation, controller tuning, and control performance evaluation. The results obtained from this analysis are returned to the PLC controller in real time.

As a result, the relatively limited computing power of PLC controllers is extended by virtually unlimited resources for data processing and storage available in the cloud or on the edge platform.

“Cloud or edge infrastructure is also an important functional component of the project because it enables data archiving. Process data stored within it is continuously collected from the PLC controller, and due to its enormous volume and high acquisition frequency, it can be classified as Big Data,”
says Dr. Eng. Patryk Grelewicz.

The project also utilizes artificial intelligence. Its role is to assess control performance based on process data collected in cloud computing resources or on a SIMATIC IPC Edge industrial edge computer. Furthermore, to optimize and accelerate development work, a digital twin of the solution was also employed.

Based on the laboratory heat distribution system, we developed a model of the system in the Siemens SIMIT environment, creating a digital twin of the laboratory heat distribution and exchange installation. Using a Siemens S7-1500 controller and SIMIT as the simulation platform, we carried out the virtual commissioning of the district heating substation control system
Dr. Eng. Michał Frątczak, Silesian University of Technology

Higher energy efficiency and lower environmental costs

The efficient operation of heat consumers has a significant impact on improving the energy performance of entire installations and also enables lower production costs in industrial plants. The solution developed by the team at the Silesian University of Technology, which uses programmable controllers and an IT infrastructure tailored to customer requirements, can support the modernization of many control systems that currently operate in a suboptimal manner.

“The process control system for heat generation and distribution developed at the Silesian University of Technology uses IT technologies for advanced control, making it possible to optimize many aspects related to energy consumption and carbon dioxide emissions. As a result, it can significantly help bridge the gap between industrial reality and Industry 4.0 technologies, while the use of the Industrial Edge platform ensures continuous and reliable operation,”
summarizes Artur Nowocień from Siemens.

Case Study - Silesian University of Technology 11

The system was developed by a project team led by Dr. Eng. Michał Frątczak.(From left: Dr. Eng. Patryk Grelewicz, Dr. Eng. Paweł Nowak, Dr. Eng. Michał Frątczak.)