Warum Because simulating at an early stage WORKS?
As a basis for the simulation of the planned WLAN infrastructure, only the floor plans of the area/route to be supplied are used. Based on the requirements recorded in advance, we simulate the WLAN propagation with all define WLAN components. These simulation results are based on assumptions and purely theoretically determined values and do not consider any potential causes of interference on site. Therefore, this form of WLAN planning is only used if the buildings to be supplied do not yet exist or cannot be accessed.
THE RESULT
You will receive a quantity structure from us that lists all the hardware you need. At this early stage, however, without information concerning the specific installation instructions for each installation site that are necessary for a proper installation.
WE SIMULATE THEORETICALLY - YOU START PRACTICALLY
The simulation includes the phases of preparation, technical execution including the measuring equipment, evaluation and post-processing.
Vorteile
- Lower financial risk than with real experiments
- Exact, repeatable tests
- Investigation of long-term effects
- Gain insights for process improvements
- Evaluation of random events
- Testing Non-Standard Distributions