Tools


Siemens Worldwide

The Magazine

Contact

Contact
The Magazine
Subscribe
The wireless transmitters are installed on the water towers to have a clear line of sight to the remote water treatment stations

Industrial communication

A rugged solution

In Georgetown, Texas, the implementation of a wireless broadband solution helped Georgetown Utility Systems save hundreds of thousands of dollars by eliminating the need to hardwire remote wastewater treatment stations to connect with the city’s fiber ring network.

Deep in the heart of Texas,  30 miles north of Austin, is historic Georgetown. The once sleepy town’s population  has almost doubled over the last  12 years, to more than 52,000. According to Ron Marrow, Georgetown Utility Systems’ transmission and distribution supervisor for SCADA, the rapid pace of growth has made providing utility services to the city an increasingly difficult task. He and his team are in charge of all communications and network connectivity across water, waste, and electrical infrastructure. Thus, they’ve been heavily involved in ongoing upgrades to meet the needs of the city’s soaring population.

Identifying inefficiencies

For years Georgetown Utility Systems used the 900-MHz radio spectrum with SCADA communications to monitor the operations of its water, sewage, and electrical distribution systems. However, as Marrow explains, with a coverage area of 300 square miles, this presented reliability issues, particularly in the summer months. “Whenever it got hotter than 90°F [32°C], communications from a remote wastewater lift station would fail,” he says. “So we’d have to send a technician to take data readings every four hours, to make sure nothing was overflowing.”

Another issue was the star topology of the city’s 900-MHz radio network. “All the remote radios were transmitting back to one central radio,” Marrow adds. “If that central radio went down, so would all our communications.” To alle viate that concern, Marrow and his team deployed a redundant 1-Gbps fiber ring network, with the intention of using its multimegabit bandwidth to eventually enable video surveillance, VoIP (Voice over Internet Protocol), and remote on-demand Wi-Fi hotspots for fieldworkers. However, before these services could be implemented, the team had to contend with a more immediate issue: cost-effectively connecting the remote water treatment stations with the city’s new fiber ring.

Living up to its name

Because in-ground fiber costs up to $25,000 per mile, extending the city’s ring to its wastewater lift stations was not economically feasible. After evaluating several options, the project team decided to employ broadband wireless – more specifically, 802.16e WiMAX, using the 4.9-GHz spectrum. WiMAX over the 4.9-GHz band would provide the range needed to reach the stations, but it did require licensing from the Federal Communications Commission (FCC) and accompanying paperwork that Marrow had no idea how to start. He did, however, know whom to call: Siemens. 

To build out the fiber ring, the Georgetown team deployed scores of RS900G Layer 2 switches from Ruggedcom, a portfolio of harsh-environment communications solutions from Siemens. The RS900G is a fully managed Ethernet switch that provides dual fiber-optic Gigabit Ethernet ports with Gigabit uplink ports and 128-bit encryption. “We already had 200 Ruggedcom devices in our network, so it only made sense to keep all the WiMAX components in the family, too,” Marrow says. “After all, they had earned their Ruggedcom name by holding up to the harsh conditions of our central Texas summers.”

The Ruggedcom point-to-multipoint 4.9 GHz WiMAXsolution provides reliable access to the data gathered in the remote water treatment stations and has saved the expense of a wired connection

The right partner

In working closely with the Georgetown team, Siemens personnel became aware of the issue of extending the fiber’s broadband throughput to the remote sites. The WiMAX technology itself also presented line-of-sight challenges, as wastewater lift stations were in low-lying areas amid Georgetown’s rolling, tree-covered terrain. To address these issues, Siemens recommended Alpha Omega Wireless, a Siemens-certified industrial wireless solution provider based in Austin.

Alpha Omega Wireless compiled a detailed set of requirements from which the company’s experts developed a Ruggedcom point-to-multipoint 4.9-GHz WiMAX solution as well as a comprehensive deployment and commissioning plan. The company also processed all the paperwork needed for the city’s FCC license to use the 4.9-GHz spectrum, saving Marrow and his team weeks of time.

Cost savings through collaboration

 “The Ruggedcom system has worked flawlessly,” says Marrow. In addition to eliminating the need to dispatch technicians to wastewater lift stations to log data by hand, Georgetown saved hundreds of thousands of dollars in capital costs by not having to lay fiber in the ground out to the remote sites. The result has been an extremely reliable, future-ready high-bandwidth wireless network.

Overall, Marrow explains that one of the biggest benefits of working with Siemens and Alpha Omega Wireless was their expertise and collaborative approach to the project. “They worked seamlessly together,” he says. “Through it all, my team and I felt like our backs were covered. No matter what issues might arise, we knew the two companies would respond as one.”

Picture credits: Siemens AG