Favor utilizar outro navegador

Parece que você está usando um navegador que não é totalmente compatível. Por favor, note que podem haver restrições na exibição do site e em sua usabilidade. Para uma melhor experiência, sugerimos que você faça o download da versão mais recente de um navegador compatível:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

Power Transmission Lines

Forward-looking solutions for electricity transmission

One result of the increasing expansion of renewable energy sources is the transformation of power generation structures. This in turn is leading to new demands on electricity transmission, and thus also on the network infrastructure. Because more electricity is being fed in from fluctuating renewable energy sources and most generation is remote from the load centers, it has become essential to reinforce and expand the network. Other key factors driving the need for network expansion include an increase in cross-border electricity exchanges between countries, the changes in conventional power station locations and increasing urbanization.

More overhead wires are not always the method of choice. The focus is increasingly on underground electricity transmission solutions. Siemens has a range of solutions on offer in this area: gas-insulated transmission lines (GIL) and extensive services for high-voltage cable systems.

Our products and services are tailored to suit your requirements. We look forward to hearing from you.
Arrange consulting appointment
Gas-insulated transmission lines
Gas-insulated transmission lines (GIL)

Gas-insulated transmission lines (GIL)

Wherever high voltages (up to 500 kV) and currents of up to 5,000 A have to be transmitted in a limited space and above-ground cables cannot be used, compact gas-insulated transmission lines (GIL) offer the technical, environment-specific and operating characteristics to provide a very good alternative.

High-voltage cable systems
High-voltage cable systems

High-voltage cable systems

Are you planning a new medium or high-voltage cable system, or expanding or converting an existing system, and are looking for a technically and financially optimized solution? We’re expert partners who can give you vendor-neutral advice and take over full responsibility for the project, from planning to commissioning.

Alternatives to overhead lines

Best solutions for efficient electricity transmission

The constantly growing need for power for both industrial and residential consumers, the integration of renewables and the increasing development of megacities all mean power networks must undergo further expansion. The decoupling of generation and consumption is making it increasingly complicated to guarantee secure and stable electricity transmission in a way that is environmentally friendly and acceptable to society. 

image

The future of electricity transmission

The existing power networks have to transport greater and greater power volumes, often coming close to their load limits. At the same time, the distances between the locations where electricity is generated and consumed are increasing, especially in the case of renewables. In Germany, for example, larger and larger wind farms are taking shape in the north of the country, and photovoltaic systems in the south, as part of the transformation to a new energy mix. All of this electricity has to be transported. 

In addition, the development of megacities and the growth in new consumers, such as in the area of electromobility, necessitate greater high-power transmission capabilities in urban centers, despite the very limited amount of space available. Situations like this will make more and more use of compact, underground transmission solutions. 

GIL installation (direct burial)
Underground power transmission via gas-insulated transmission lines

Underground power transmission will help protect the appearance of the landscape, reducing the visual impact. At the same time, underground transmission will considerably reduce the amount of land required. 

High performance along narrow routes

High-power electricity transmission poses a major challenge for project developers and planners: their objective is to guarantee a secure, reasonably priced and environmentally friendly electricity supply. In some regions, there may also be societal challenges: public acceptance of large-scale power lines is often minimal, and this is where an underground arrangement may prove the more appropriate solution. In larger cities and in the vicinity of central infrastructure complexes such as airports, there is often insufficient space for extensive overhead lines, and here, too, compact underground solutions prove the method of choice. 

References

Success Stories

If overhead lines are not an option for electricity transmission, the lines must be laid below ground. Siemens has successfully implemented many electricity line projects for customers in more than 20 countries, and offers a complete portfolio of solutions for gas-insulated transmission lines (GIL) and high-voltage cable systems.

image
image

Downloads, support and services

Additional information

This is where you can find our brochures, contact details for individual consulting interviews and further information.

Power Transmission Service

Siemens support the development of the power transmission and distribution grid with its strong team of experts and a number of services

Learn more

Power Transmission Service

Siemens support the development of the power transmission and distribution grid with its strong team of experts and a number of services

Learn more

Technical solutions

Environmentally friendly electricity transmission

It is becoming more and more important – and more and more costly – to transmit electricity securely over long distances. That applies especially to transmitting electricity underground with high power densities and minimum impact on the environment. In addition to technically optimized and reliable solutions for low-loss transmission, it is essential to gain acceptance from the local population when constructing and modernizing transmission lines. Siemens has the right portfolio of solutions for every challenge, all individually tailored to suit your needs.

image
Expand your knowledge with our free White Paper
Download White Paper