Please use another Browser

It looks like you are using a browser that is not fully supported. Please note that there might be constraints on site display and usability. For the best experience we suggest that you download the newest version of a supported browser:

Internet Explorer, Chrome Browser, Firefox Browser, Safari Browser

Continue with the current browser

A fail-safe electrical system

Avoiding interruptions in supply in an electrical system as extensive and complex as Brazil’s is a challenge. The answer: intelligent solutions that control and interconnect, from the generation to the great consumer centers.

 

Intelligence in the interconnected system


Boosting the economy with reliable energy

The National System Operator (ONS) was faced with an imperative need: increasing the degree of the Brazilian electricity system security, to keep up with the pace of economic growth and to avoid supply failures. The challenges were many: the continental dimensions of Brazil, the variations in consumption from one region to another, and the distance from the major urban centers of the main generating poles.

image

Minor Risks, Improved Management


The way to meet the challenge was the creation of the Energy Management Network (REGER). The concept behind the Reger project is a unified, modern and dynamic platform, structured on a large computer system that integrates the four regional operation centers and the national ONS center, allowing the increase of management efficiency and greater system security . The unified platform enables the operator to "see", in real time, the dynamics of consumption, adjusting the generation and the transmission for the safe supply of energy.


REGER's computational architecture, which promotes the improved integration of the performance of various control centers, represents an important quality leap in the operation of transmission and power generation systems, mitigating the risk of interruption in the power supply, bringing more reliability and Making it a model of operation for the world.

 

But there is another benefit as important as reducing the risks of supply disruptions: integrating the national center and the four ONS regional operation centers, Reger system provides comprehensive data sharing and redundancy, ensuring continuous supervisory and control capabilities. And this condition is ensured even in extreme situations, such as the loss of an operations center. In practice, this allows more agile decision making, greater reliability and reduced risk of shortages in the transmission system.


A further step in this scenario is the implementation of energy efficiency projects, optimizing available resources (generation sources, transmission lines and distribution systems, for example).


Set up in a consortium formed by Siemens and Cepel (Centro de Pesquisa de Energia Elétrica), Reger, in full operation since 2013, has as its main components the SCADA (Supervisory Control and Data Acquisition) platform containing EMS (Energy Management System) For real-time grid analysis and the innovative "Evergreen" concept that keeps the system up to date with the latest technology.     

National System Operator

Supervision and control system (SCADA - Siemens), integrating the four regional centers of the National System Operator and the national center.

Integrated Regional Centers

Recife

Brasília

Rio de Janeiro

Florianópolis

Operating Features

Example of implanted and evolving operation supporting tools.

Fire Detection
System

One of the tools to support the operation of the National Interconnected System is the fire detection system, which is part of the safety enhancement plan for the operation of the SIN.

Operating Features

Example of implanted and evolving operation supporting tools.

Lightning
detection system

A new system deployed from the Reger project can also anticipate the possibility of lightning in specific regions, which have the potential to disrupt power supply.

Operating Features

Example of implanted and evolving operation supporting hardware.

Weather
forecast

Through the analysis of data of the meteorological forecast, the new tools of the National Interconnected System are able to predict climate changes that could harm supply, indicating mitigation actions.

image

New control rooms

CNOS/COSR-NCO Brasília-D

In Brasilia, there is the Central Operation Center and also the structure responsible for coordinating and controlling the operations of the National Interconnected System in the Central-West Region.

image

New control rooms

COSR-SE Rio de Janeiro-RJ

The Southeast Operations Center, located in Rio de Janeiro, has more than 1,200 operating documents available and about 2,100 diagrams always updated, like the other four centers.

image

New control rooms

COSR-NE Recife-PE

In the Northeast, control and coordination are carried out at the Recife Operation Center, which, like the other four centers, uses a telecommunications system with availability equal to or above 99.98%.

image

New control rooms

COSR-S Florianópolis-SC

The ONS Operations Center of the Southern Region is located in Florianópolis (SC). Its function is to coordinate and control the operation of the generation and transmission facilities of the National Interconnected System (SIN).