Water scarcity affects one in three people globally, and climate change and population growth are only adding to water stress. Siemens' state-of-the-art water-reuse technologies provide compelling answers to the problems of water-supply conservation, management and protection. Water reuse conserves limited potable water supplies by using treated wastewater effluent for non-potable uses such as irrigation and use in industrial processes. Reusing water is a sustainable way of preserving a municipality's supply of drinking water. Siemens’ biological treatment, membrane filtration and separation, physical and chemical treatment and ultraviolet (UV) system technologies are all helping to provide a sustainable solution for communities and industries alike. An example of the successful use of Siemens' technology is the membrane bioreactor (MBR) system at the Beixiaohe plant in China, which provides 64 MLD of irrigation and utility water. Additionally, the Changi Water Reclamation Plant (WRP) in Singapore features Siemens’ odor control, primary and secondary wastewater treatment equipment and a full-scale MBR testing facility. It also features seven Memcor® membrane filtration systems for the Changi NEWater plant that is located on the roof of the Changi WRP. The WRP reclaims more than 28 million cubic feet (800,000 m3) a day of wastewater.
Besides water reuse, seawater desalination may also be a viable solution for coastal communities with current or projected water-supply problems. Siemens' solutions in this area include membrane filtration as pretreatment to reverse osmosis (RO). This technology is growing in popularity because of its small system footprint and reliable output quality. A large desalination project in Australia is using Memcor® ultrafiltration membranes for this application.
Furthermore, we are now developing advanced desalination technology at our R&D center in Singapore. This will reduce energy consumption by at least 50% compared with existing desalination processes.
| Customer Value |
| Reduced costs |
| Reduced space requirements |
| Ability to supply growing populations and expanding industry |
| Environmental Value |
| Reduced water stress |
| Lower wastewater emissions |
| Reduced reliance on scarce water resources |
2011-Feb-25 | Author