Rail still has a major role to play in sustainable mobility. Growing environmental awareness and new logistics strategies are helping to make national and international rail transportation increasingly important. Rail traffic accounts for just 2 percent of the 28 percent of energy consumed as a whole by transportation worldwide. This means that, alongside investing in the expansion of the rail networks, deploying energy-saving low-emission trains represents the best way forward for eco-friendly freight, regional and intercity traffic.
With Vectron, Siemens has created a locomotive that offers numerous advantages. Available in electric and diesel-electric versions, this modern engine is nothing if not versatile. Throughout its operating life, it can be converted quickly and flexibly to different operating roles and requirements anywhere in Europe.
Designed with an eye to today’s strict regulations on pollutants, particulate matter and noise in many European countries, Vectron is the first diesel-electric engine to be fitted as standard with the very latest diesel engine and particulates filter, which means its particulate emissions are up to 87.5 percent lower and conform to limits defined in Europe’s EU97/IIIB standard. Like all Siemens diesel locomotives, Vectron is also well within the noise limits set by the European TSI Noise standard: its stationary and starting noise levels are 10 decibels below the defined maximums. The electric versions of Vectron are equipped with a highly efficient system for recovering braking energy and feeding it back into the power system. This and their low standby energy consumption and generally improved system design make them especially economical.
Vectron locomotives are built in energy-saving manufacturing locations using environmentally safe materials. They are also 98 percent recyclable (94 percent material recovery, 4 percent thermal recovery) – a figure that’s nothing less than exemplary.
| Country packages included as standard for borderless mobility |
| Future-proof thanks to lifelong convertibility |
| Traffic mission-oriented portfolio for long-term cost efficiency |
| Needs-based service for highest availability |
| High performance based on many years of locomotive expertise |
| Compliance with European emissions limits |
| Built with eco-friendly materials |
| Braking energy recovered is fed back into power system and used to support auxiliary equipment and train power supplies |
| Use of water-soluble paints |
| 98-percent recyclable |
2011-Mar-03 | Author