Coal-fired power plants are among the world’s biggest carbon dioxide emitters, and as countries work toward their 2012 Kyoto Protocol greenhouse gas targets, plant operators are seeking to reduce their carbon footprints significantly. Siemens offers cutting-edge technology designed specifically for existing coal-fired steam-turbine power plants that helps to boost their efficiency. Modernization and upgrades offer these plants a means of substantially reducing their carbon output without investing a lot of money.
RWE Power AG, for instance, has commissioned Siemens to modernize the Niederaussem steam power plant in the German state of North Rhine-Westphalia. With the aid of state-of-the-art turbine technology, the plant has succeeded in cutting its carbon dioxide emissions by 600,000 tons per year while continuing to produce the same amount of electricity. This has largely been achieved by boosting efficiency. By 2020, the efficiency of new coal-fired generating facilities should surpass the 50-percent mark, up from 47 percent currently. Equipping all of the world’s coal-fired plants with state-of-the-art technology could lower carbon dioxide emissions by 1.7 billion tons per year.
To utilize fuel as efficiently as possible, fossil power plants need to operate in an optimum thermodynamic range and avoid unnecessary startups and shutdowns. The Energy Management Suite (EMS), an IT solution from Siemens, helps plant operators to accomplish this, thereby saving fuel and reducing emissions.
| Modernization and upgrades improve efficiency by more than 2 percent on average |
| More output with the same amount of fuel (38 megawatts in the case of Mehrum coal-fired power plant) |
| Longer maintenance cycles |
| Extended service life for the overall plant |
| State-of-the-art turbine technology has enabled Niederaussem steam power plant to cut its carbon dioxide emissions by 600,000 tons per year without reducing its power output |
| Specific emissions of other air pollutants are also lower |
| Sizeable carbon dioxide reduction in relation to investment |
2011-Feb-28 | Author