less electricity compared to conventional electric arc furnaces
If ever an entire site was fully committed to an innovation project, Siemens VAI Metals Technologies in Willstätt-Legelshurst is it. As the Siemens center of competence for Electric Steelmaking Plants for Long Products, the facility located in the small German village close to the French border is a hotbed of steelmaking innovation. Now they have done it again – with the new SIMETAL EAF Quantum, a highly energy efficient and eco-friendly electric arc furnace (EAF). The first unit will go into operation in 2013.
Global demand for steel continues to grow. However, iron and steelmaking account for roughly 20 percent of the world’s industrial energy consumption and 30 percent of industrial CO2 emissions. The power consumption of electric arc furnaces used for melting scrap metal is particularly high.
Ever the trailblazers, a group of seven engineers at the site got together in 2009 to design an electric arc furnace capable of increasing total output while reducing energy consumption and greenhouse gas emissions. The SIMETAL EAF Quantum was born – a quantum leap in furnace efficiency.
The team came up with a promising design and presented it to the management. That’s when things really took off. “We saw great potential in the new furnace concept for our customers and immediately decided to prioritize the project,” site CEO Bertram Junker recalls. News of the plans for the new furnace was enthusiastically welcomed by the staff of more than 320 employees, including engineers, specialists and support personnel. It has become a rallying point for the entire site,” as Dr. Markus Dorndorf, Head of R&D, points out. “Everyone is totally committed to the project.”
Steelmaking innovation has a long tradition at Willstätt-Legelshurst. The Quantum electric arc furnace is the centerpiece of the new compact steelmaking plant Siemens is constructing for the Mexican steelmaker Talleres y Aceros S.A. de C.V. (Tyasa) at its Ixtaczoquitlán site. It achieves tap-to-tap times as low as 36 minutes. At just 280 kilowatt-hours per ton of crude steel, it consumes up to 20% less electricity compared to conventional electric arc furnaces. Tyasa CEO Oscar Chahin Trueba underscores this factor in stating: “We’re expecting to gain significant advantages in operating costs, especially from the new electric arc furnace.” There is another significant advantage: 30% lower CO2 emissions.
While some of the staff at the site are feverishly working to implement the new Tyasa furnace, others are already tinkering with new concepts to further improve furnace efficiency. What will they think up next?
2011-Feb-23 | Author