Skip to main content

Why SINUMERIK CNC Robotics?

CNC-controlled robotics allows a smarter path to automation. A single SINUMERIK platform reduces engineering effort, simplifies integration, and eliminates the friction of working with multiple systems. This means stable interfaces, easier commissioning, and predictable performance across the entire robot workspace. It delivers higher machine availability, more consistent quality, and workflows that existing CNC-trained experts can easily handle.

Meet SINUMERIK Machine Tool Robot

At the forefront of CNC Robotics stands the SINUMERIK Machine Tool Robot (MTR) —the world’s most precise machining robot. MTR combines a revolutionary drive concept with advanced SINUMERIK motion control. This breakthrough makes high-force applications, including machining steel, feasible within the robot cell.

Breakthrough Performance

Absolute path accuracy improved by over 200% and up to 40% productivity increase​.

Enhanced Rigidity

Higher dynamic stiffness in the entire working area allows demanding machining tasks in steel with high process forces.

Extended Application Fields

High-precision use cases – also without process forces – such as additive manufacturing (AMF) and inkjet printing, laser and waterjet cutting benefit from the achievements.

Getting started with SINUMERIK CNC Robotics

SINUMERIK CNC Robotics system contains multiple building blocks that work seamlessly together. This section provides an overview of the core components that form the full system. These elements enable precise, reliable, and fully integrated robotic automation for path control motions.​

Discover how others use SINUMERIK CNC Robotics

Select...

With SINUMERIK‑controlled robot kinematics, milling operations can be programmed and executed just like on a traditional CNC machine. The controller ensures precise path accuracy, coordinated multi‑axis interpolation, and stable performance even on complex geometries.

Frequently asked questions