Industry Sector / Metals Technologies
Linz, 2013-Apr-17
Siemens Metals Technologies has received an order from ArcelorMittal South Africa – Saldanha Works, to modernize the controllers of the two Gimbal charging systems in a Corex plant of the company. The Simatic-based Gimbal Controllers will replace systems which have been in use since 2004 and 2006, respectively. Their range of functions will be transferred to a Siemens platform and expanded. The new controllers will ensure smooth movement of the chutes, subject only to low mechanical forces, allowing the charge to be distributed precisely and dynamically in many different charging patterns.
A Corex C-2000 plant has been in operation at ArcelorMittal South Africa's Saldanha Works since the end of 1998. Two Gimbal charging systems charge the oxide into the reduction shaft, and the coal into the melter gasifier, respectively. The new controllers will enable the chutes to be moved smoothly with low mechanical forces, and so distribute the raw materials precisely. The process engineer will be able to define not only standardized distribution patterns, such as rings, but also any desired pattern with the aid of the "Free Shape" function, for example offset ellipses, clover-leaf patterns and kidney shapes. This will allow geometric and/or process asymmetries to be compensated and improve process operation.
The Gimbal automation system is based on rugged, industrially proven components from Siemens. The modular hardware platform will be complemented by a standardized programming environment. The operator and monitoring system has been expanded to include extensive diagnostic and condition monitoring functions. These include, for example, the detection of loss of the chute, impermissible pressures, electric short circuits, cable breaks and sensor faults. Important operating and diagnostic data are also displayed to the plant personnel on a Simatic Mobile Panel. This makes maintenance considerably easier. For example, hydraulic cylinders can be centered locally, valves can be checked or various process values can be displayed and subjected to a trend analysis. The Gimbal Controllers are scheduled to be commissioned for real plant operation in August this year.
Further information about solutions for steel works, rolling mills and processing lines can be found at www.siemens.com/metals.
Follow us on Twitter: www.twitter.com/siemens_press
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Metals Technologies Business Unit (Linz, Austria), part of the Siemens Industry Sector, is one of the world's leading life-cycle partners for the metallurgical industry. The Business Unit offers a comprehensive technology, modernization, product and service portfolio as well as integrated automation and environmental solutions covering the entire life cycle of plants. For more information, visit http://www.siemens.com/metals
Reference Number: IMT201304352e
Turmstr. 44
4031 Linz
Austria
Tel: +49 (9131) 7-44544