Industry Sector / Metals Technologies
Linz, Austria, 2013-Mar-06
Siemens Metals Technologies has equipped two long rolling mills belonging to BGH Edelstahlwerke GmbH with new drive and automation equipment. The wire rod mill in Freital was modernized for BGH Edelstahl Freital GmbH, and the flat bar line in Katowice, Poland, was brought up to the state-of-the-art for BGH Polska Sp.z o.o. Both BGH plants now employ end-to-end automation solutions based on Simatic S7 and Siroll LR, which enable simplified plant operation and maintenance as well as increased availability. The modernization projects were completed alongside each other in just twelve months, with conversion activities taking only three weeks in each case.
BGH Edelstahlwerke GmbH is a medium-sized steelmaker based in Freital, Saxony. The holding includes seven autonomous production locations in Germany and Poland. The company runs an electric-arc-furnace-based minimill meltshop in Freital, in which liquid steel can be cast either as blocks or billets. These are then further processed in a blooming mill and a wire rod line. Siemens replaced the existing automation technology on the continuous rolling mill and cooling bed with Simatic S7 programmable logic controllers, and installed new application software based on Siroll LR. The ancillary plant equipment, such as the bar handling, Garrett coiler and laying head, is now controlled by Step 7 software, and Siroll LR functions have been added for the drive control, for example. Simatic WinCC was also installed as the new operator control and monitoring system.
The BGH rolling mill in Katowice consists of a two-high reversing mill, a 5-stand flat rolling block, and a 16-stand continuous rolling mill. It also has heat treatment and finishing sections. The rolling lines produce squares and flat bars with cross-sections ranging from 15 x 15 to 250 x 70 millimeters. VAI supplied the continuous rolling mill in 1998. The automation hardware for the rolling line, cooling bed and induction furnace has been completely converted to Simatic-S7 controllers, and the existing Step-5-based application software and the GFM CNC 6000 technological control systems have been replaced with a Siroll LR solution. Simatic PCS7 is used as the process control and visualization system. The Siroll LR Tool Roll Master has been brought up to the state-of-the-art to optimize the rolling sequence control. In addition, the drive system control units were replaced with Sinamics DCM control modules, which enabled the drives to be easily integrated into the new automation environment while retaining their existing power sections, thus reducing investment costs.
Siemens was responsible for engineering, supplying, installing and commissioning the new equipment in both projects.
For further information on solutions for steelworks, rolling mills and processing lines, please see www.siemens.com/metals
Follow us on Twitter at: www.twitter.com/siemens_press
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Metals Technologies Business Unit (Linz, Austria), part of the Siemens Industry Sector, is one of the world's leading life-cycle partners for the metallurgical industry. The Business Unit offers a comprehensive technology, modernization, product and service portfolio as well as integrated automation and environmental solutions covering the entire life cycle of plants. For more information, visit http://www.siemens.com/metals
Reference Number: IMT201303355e
Turmstr. 44
4031 Linz
Austria
Tel: +49 (9131) 7-44544