Industry Sector / Industry Automation Division
Nuremberg, 2013-Apr-02
Siemens Industry Automation Division has extensively revised its network management software Sinema Server. The new version 12 allows each Sinema Server station to monitor up to 500 devices, i.e. double the number of clients monitored by its predecessor. Moreover, as each Sinema Server can display the status of up to 100 other Sinema Servers within the network, the total number of clients that can be monitored by Siemens application the is 50,000. Connected components are automatically identified via SNMP (Simple Network Management Protocol) and Profinet devices via DCP (Device Control Protocol). The new version 12 also allows the user to edit, load and save device profiles. Moreover, the user interface has been enhanced and the integration into HMI devices and Scada systems such as Simatic WinCC or Simatic PCS7 greatly improved.
Sinema Server has been designed to continuously monitor Ethernet and Profinet networks in industrial and infrastructure environments. The software displays all physical connections at port level as well as machine- or application specific network configurations. The application flags up any malfunction within the network, thereby assisting with rapid fault-location and removal, which in turn, lead to reduced downtime. In order to do this, Sinema Server creates an image of the network topology including any existing VLANs (Virtual LANs). This enables the software to then continuously monitors both changes in the network architecture and the availability and status of components and connections within the network. This is possible even for network sections which are protected by security products provided they have been cleared for access by Sinema Server. The device diagnostics function provides configuration and identification data such as name, device type, serial number and product-specific status values. Sinema Server V12 also allows users to define alarm threshold values for the various parameters of a specific device. Sinema Server can be used not only for monitoring but also for documenting device inventory, network availability and network utilization.
Sinema Server V12 supports Windows XP, Windows 7 (32/64 bit) and Windows Server 2008 R2. Users are now free to choose from four display languages: English, German, French or Chinese.
For more information on Sinema Server, please visit www.siemens.com/sinema
Follow us on Twitter: www.twitter.com/siemens_press
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Siemens Industry Automation Division (Nuremberg, Germany) supports the entire value chain of its industrial customers – from product design to production and services – with an unmatched combination of automation technology, industrial control technology, and industrial software. With its software solutions, the Division can shorten the time-to-market of new products by up to 50 percent. Industry Automation comprises five Business Units: Industrial Automation Systems, Control Components and Systems Engineering, Sensors and Communications, Siemens PLM Software, and Water Technologies. For more information, visit http://www.siemens.com/industryautomation
Reference Number: IIA2013043418e
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895 7975