Industry Sector / Industry Automation Division
Nuremberg, 2013-Apr-08
The Siemens Industry Automation Division has extended its range of temperature sensors to include the SITRANS TS product family. The new resistance thermometers and thermocouples are designed for universal use. The device line has a modular design, and offers a large range of sizes, materials, sensors and transmitters. It not only supports the central communication standards HART, PROFIBS PA and Foundation Fieldbus, but is also certified under ATEX and IECEx, which enables the devices to be used worldwide. SITRANS TS is therefore suitable for both basic and highly demanding applications throughout the entire process industry.
The modular SITRANS TS product family consists of the three product lines SITRANS TS100, TS200 and TS500. They are suitable for a wide range of applications in the process industry, such as in the fields of chemicals, oil, gas and power. The product portfolio is clearly structured. Certain designs are certified under ATEX and IECEx as being flameproof for gas and dust, intrinsically safe, and Ex n. This has advantages for globally active users, especially in the fields of logistics, inventory management and documentation.
The SITRANS TS100 and TS200 product series are available as cable and compact thermometers. This makes them especially suitable for universal use, such as detecting the temperatures of machine bearings. The compact insertion thermometers can also be used in confined spaces, and their mineral insulated design makes them not only flexible but also resistant to vibrations and high temperatures up to +1,100 degrees Celsius. The SITRANS TS500 product line is designed for applications with low to high process stresses. A selection of protective tubes made of solid or welded pipe material is available for this purpose. The user can use a wide range of process connections, connection heads, sensor types, transmitters and displays to configure individual solutions for a process. The optional 4 to 20 mA transmitters, HART, PROFIBUS PA and Foundation Fieldbus enable devices to be easily integrated into the operating tools of process control systems, such as SIMATIC PDM.
Further information on temperature sensors is available at www.siemens.com/sitranst
Follow us on Twitter: www.twitter.com/siemens_press
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Siemens Industry Automation Division (Nuremberg, Germany) supports the entire value chain of its industrial customers – from product design to production and services – with an unmatched combination of automation technology, industrial control technology, and industrial software. With its software solutions, the Division can shorten the time-to-market of new products by up to 50 percent. Industry Automation comprises five Business Units: Industrial Automation Systems, Control Components and Systems Engineering, Sensors and Communications, Siemens PLM Software, and Water Technologies. For more information, visit http://www.siemens.com/industryautomation
Reference Number: IIA2013043407e
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895-7975