Industry Sector / Industry Automation Division
Nuremberg, 2013-Mar-26
Siemens Industry Automation Division expands its offer for heating control systems with the compact Siplus HCS3200 system. In its rugged, totally enclosed housing with degree of protection IP65, Siplus HCS3200 is protected against dust and dirt and can therefore also be mounted outside the cabinet near to the heating elements. The connections for up to nine heating elements in the mid power range up to 4kW and for an external fan are easily accessible at the bottom of the device. The areas of application for the heating control system are primarily distributed applications with a high degree of protection, for example the production of PET bottles, in which preforms are heated or the drying of coatings for wheel rims in the automotive industry. Siplus HCS3200 marks a new generation of Siemens heating control systems: The new enclosure concept combines all functionalities in a single device and reduces the space requirement compared with a conventional assembly with individual components by 50 percent.
Siplus HCS3200 also provides detailed and intelligent diagnostics functions. This enables faults in the heating process to be located faster, thus increasing plant availability. The system is also integrated into the TIA environment and can easily be integrated into existing automation systems with Siemens components. Configuration can be performed quickly and simply via STEP 7 or the TIA Portal.
Over the next few years, further models will successively expand and modernize the Siemens product line for heating control systems.
You will find more information on the Siplus heating control system at www.siemens.com/siplus-hcs
Follow us on Twitter at: www.twitter.com/siemens_press
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Siemens Industry Automation Division (Nuremberg, Germany) supports the entire value chain of its industrial customers – from product design to production and services – with an unmatched combination of automation technology, industrial control technology, and industrial software. With its software solutions, the Division can shorten the time-to-market of new products by up to 50 percent. Industry Automation comprises five Business Units: Industrial Automation Systems, Control Components and Systems Engineering, Sensors and Communications, Siemens PLM Software, and Water Technologies. For more information, visit http://www.siemens.com/industryautomation
Reference Number: IIA2013033419e
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895-7945