Energy Sector / Fossil Power Generation Division
Erlangen, 2013-Apr-25
Siemens Energy and its consortium partner GS E&C have completed and commissioned the two turnkey combined-cycle power plant (CCPP) projects Sohar 2 and Barka 3 in the Sultanate of Oman on schedule. In 2012, both units went into operation in simple-cycle mode to help meet the country's strongly growing demand for electric power. Following steam turbine add-ons, both plants have commenced commercial operation in combined-cycle configuration in April 2013 – well in time to meet the peak electricity demand during the hot summer months. With their total electrical generating capacity of 1.5 GW, these two plants increase the Sultanate's current existing capacity of circa 4.5 GW to approximately 6 GW.
Sohar 2 was built in the Sohar industrial park approximately 200 kilometers northwest of the nation's capital, Muscat, while Barka 3 was erected in the immediate vicinity of Muscat. For each of these plants, Siemens supplied the main components comprising two SGT5-4000F gas turbines, one SST5-5000 steam turbine, three SGen5-2000H generators, the electrical equipment and the SPPA-T3000 instrumentation and controls system. The consortium partner GS E&C supplied the heat recovery steam generators and was responsible for other scopes such as the civil construction work, electrical transformers and ancillary systems as well as equipment installation.
Siemens has been active in Oman since 1974, playing an important part in many of Oman's major power plant projects over the past 40 years. "As an EPC partner, our customers can benefit from our expertise in integrating the mechanical, electrical and chemical processes of fossil fuel power plants," says Lothar Balling, head of Gas Turbine Power Plant Solutions at Siemens Energy's Fossil Power Generation Division. "At both Sohar 2 and Barka 3, we succeeded on schedule in achieving reliable technological excellence by wedding quality in project planning and project execution."
Purchaser of the project-financed plants was a consortium led by the French utility GDF SUEZ. Al Batinah Power Company is the owner of Sohar 2 Power Station, while Al Suwadi Power Company owns Barka 3. The two plants will be operated by Suez-Tractebel Operation and Maintenance Oman LLC (STOMO).
Highly efficient combined cycle power plants are part of Siemens' Environmental Portfolio. In fiscal 2012, revenue from the Portfolio totaled about €33 billion, making Siemens one of the world's largest suppliers of ecofriendly technologies. In the same period, our products and solutions enabled customers to reduce their carbon dioxide (CO2) emissions by more than 330 million tons, an amount equal to the total annual CO2 emissions of Berlin, Delhi, Hong Kong, Istanbul, London, New York, Singapore and Tokyo.
For further information on Gas Turbine SGT5-4000F, please see www.siemens.com/energy/SGT5-4000F
Follow us on Twitter at: www.twitter.com/siemens_press
The Siemens Energy Sector is the world's leading supplier of a broad spectrum of products, services and solutions for power generation in thermal power plants and using renewables, power transmission in grids and for the extraction, processing and transport of oil and gas. In fiscal 2012 (ended September 30), the Energy Sector had revenues of EUR27.5 billion and received new orders totaling approximately EUR26.9 billion and posted a profit of EUR2.2 billion. On September 30, 2012, the Energy Sector had a work force of almost 86,000. Further information is available at: http://www.siemens.com/energy
Reference Number: EFP201304029e
Freyeslebenstr. 1
91058 Erlangen
Germany
Tel: +49 (9131) 18-85753