Joint press release from Siemens and Stadtwerke München
Nuremberg / Munich, Germany, 2012-Apr-04
Stadtwerke München (SWM, Munich City Utilities, Germany), has jointly with Siemens Infrastructure & Cities created a virtual power plant in which a number of small-scale, distributed energy sources are pooled and operated like a single installation. The main aim of SWM is to improve the reliability of planning and forecasting for decentralized power generation sources in the area which it supplies, by means of this virtual power plant devised jointly with Siemens. In the first stage, unit-type cogenerating stations with a total rating of eight megawatts (MW) were integrated, along with renewable energy generating plants amounting to twelve MW. The core component of this virtual interconnection is the Distributed Energy Management System DEMS from Siemens. It ensures that Stadtwerke München can not only optimally deploy and operate its decentralized energy sources and loads, but also add more value from greater marketing scope.
SWM's virtual power plant, in which six unit-type cogeneration modules, five hydropower plants and a wind farm in the Munich area have been combined to form a virtual interconnection, can be operated more efficiently than the decentralized plants separately. "We are in a position to create a virtual power plant as a key element of a Smart Grid in such a way as to provide maximum possible benefit for the operators of the integrated distributed energy sources and for the power supplier too. For municipal utilities, virtual power plants offer new potential", commented Jan Mrosik, CEO of the Smart Grid Division of the Siemens Infrastructure & Cities Sector.
"The virtual power plant meets the demands encountered in both operation and marketing. It enables SWM to add more value, because it opens up further marketing alternatives, for example on the Leipzig Energy Exchange EEX or the market for regulated energy. Our initial positive experience is encouraging us to expand the virtual power plant by including further energy sources and switched loads. In the long term this will create prospects for counteracting the supply problems that arise when more of the infeed comes from renewable energy sources. That is precisely what a Smart Grid is all about", said Stephan Schwarz, SWM Director for Utilities and Technology.
On the basis of sophisticated information and communication technology, the distributed energy management system DEMS from Siemens networks and pools the individual distributed energy sources, so as to be able to control them centrally as one virtual power plant. The system processes all the important information such as weather forecasts, current electricity prices and energy demand. Based on these data, a deployment schedule for all included plants is drawn up and monitored. For example, thermal loads are predicted depending on weather forecasts and day type in hourly time resolution. The anticipated level of generation from renewable energy sources is based on weather forecasts and on the respective plant characteristics. The calculated deployment schedule consequently minimizes the costs of generation and operation in the interconnected plants making up the virtual power station. The DEMS takes account of ecological as well as economic aspects.
In the context of real-time optimization and on the basis of the deployment schedule, deviations from plan that occur in the course of system management are allocated to generation, storage and controllable loads, so that overall planned targets can be met. The software-based distributed energy management system is connected to the process via the Siemens Simatic WinCC HMI. For the exchange of individual values and ranges thereof between DEMS and the components involved, standardized TCP-IP data interfaces are used. As communication takes place via LAN or WAN, GPRS, bus systems or ISDN lines, the existing communications infrastructure of the operator of the virtual power plant can be utilized.
The Siemens Infrastructure & Cities Sector (Munich, Germany) with approximately 87,000 employees, offers sustainable technologies for metropolitan areas and their infrastructures. Its offerings include integrated mobility solutions, building and security technology, power distribution, smart grid applications, and low- and medium-voltage products. The Sector comprises the Divisions Rail Systems, Mobility and Logistics, Low and Medium Voltage, Smart Grid and Building Technologies. For more information, visit http://www.siemens.com/infrastructure-cities
The Siemens Smart Grid Division (Nuremberg, Germany) supplies power providers and network operators, industrial enterprises, infrastructure elements and cities with products and solutions for intelligent and flexible network infrastructures. To meet growing energy needs, the networks of today and tomorrow must integrate more and more renewable energy sources and ensure bi-directional energy and communication flows. Smart Grids help make it possible to generate and use power efficiently and on demand. For more information, visit
http://www.siemens.com/smartgrid
Stadtwerke München (SWM), Munich's municipal utilities company, is one of the largest energy and infrastructure companies in Germany. Over one million private households, SMEs and business clients benefit from the services provided by SWM on a daily basis. For decades, SWM has provided energy (electricity, natural gas, district heating) for the Bavarian capital in a safe and environmentally benign way. Furthermore, SWM supplies the megacity with fresh drinking water from the Bavarian Voralpenland and with 18 indoor and outdoor swimming pools they operate one of the most modern bathing environments in Germany. The MVG transport subsidiary is responsible for the underground, bus and tram systems and therefore a significant pillar in Munich's public transport network. SWM employs around 7,750 staff and in the 2010 fiscal year turnover reached around 3.8 billion euros. Further information is available at: www.swm.de/english.html
Reference Number: ICSG201204017e
Humboldtstr. 59
90459 Nuremberg
Germany
Tel: +49 (911) 433-8617