Healthcare Sector / Clinical Products Division
Erlangen, Germany, 2012-Nov-26
At the 98th Scientific Assembly and Annual Meeting of the Radiological Society of North America (RSNA) in Chicago, Siemens Healthcare is introducing the Acuson Freestyle ultrasound system that features wireless transducers, eliminating the impediment of cables in ultrasound imaging. To enable this pioneering technology, the system brings to the market a large number of innovations, including acoustics, system architecture, radio design, miniaturization, and image processing. The development of wireless ultrasound is in line with the objectives of the Healthcare Sector's global initiative Agenda 2013, specifically in the areas of innovation and accessibility. The Acuson Freestyle system will expand ultrasound's use in interventional and therapeutic applications, where the technology provides numerous workflow and image quality advantages.
Transducer cables have always been a cumbersome necessity in ultrasound imaging. Not only are they an impediment to fast and ergonomic examination procedures, but they also present an infection control risk in sterile interventional settings, even when they are covered in sterile sheaths. "Siemens Healthcare is the first company to introduce an ultrasound system that enables physicians to work with cable-free transducers," said Jeffrey Bundy, CEO of the Siemens Healthcare Ultrasound business unit. "The Acuson Freestyle system facilitates the use of advanced ultrasound technology into clinical fields requiring a sterile environment, such as interventional radiology, anesthesiology, critical care, cath lab, or emergency care." Wireless transducers can also expand ultrasound into new and emerging applications, such as administering nerve blocks, enhancing vascular access, and improving target localization through ultrasound guidance during therapeutic interventions and biopsies.
For image acquisition and processing, the Acuson Freestyle system employs advanced synthetic aperture imaging technology, an integration of proprietary hardware and software, which was specifically developed for the wireless signal transmission of full-resolution digital image data at very high data rates. Focusing on each pixel in the image, this method produces excellent image quality throughout the field of view. This design reduces the transducer's power requirements, increasing battery life. Wireless real-time ultrasound data transmission is further enabled through the proprietary development of a novel ultra-wideband radio technology, which, operating at a high frequency of 7.8 gigahertz, is not susceptible to interference with other electronic equipment.
Three wireless transducers are available for the Acuson Freestyle system, covering a range of general imaging, vascular, and high-frequency applications such as musculoskeletal and nerve imaging. The user can operate the transducers up to three meters away from the system, which includes an ergonomic interface that enables remote control of scanning parameters from within the sterile field. The Acuson Freestyle system has a 38-centimeter, high-resolution LED display. The system console can be mounted easily on a lightweight cart and also operates on battery power.
Launched in November 2011 by the Siemens Healthcare Sector, "Agenda 2013" is a two-year global initiative to further strengthen the Healthcare Sector's innovative power and competitiveness. Specific measures will be implemented in four fields of action: Innovation, Competitiveness, Regional Footprint, and People Development.
Press pictures of the new Acuson Freestyle are available at: www.siemens.com/healthcare-pictures/Freestyle
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 51,000 employees worldwide and operates around the world. In fiscal year 2012 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 1.8 billion euros. For further information please visit: http://www.siemens.com/healthcare
The products mentioned here are not commercially available in all countries. Due to regulatory reasons the future availability in any country cannot be guaranteed. Further details are available from the local Siemens organizations.
Reference Number: HCP201211006e
Henkestr. 127
91052 Erlangen
Germany
Tel: +49 (9131) 84-6188
This press release was updated on 04.12.2012 at 2:15 PM CET.