Healthcare Sector / Clinical Products Division
Erlangen, Germany, 2012-Nov-26
Siemens Healthcare is launching the Mammomat Inspiration Prime Edition – the first mammography system that lowers patient dose up to 30 percent without compromising image quality. The Mammomat Inspiration Prime Edition lowers dose by replacing the standard scatter radiation grid with a new algorithm for progressive image reconstruction. This new algorithm identifies scatter-causing structures and calculates a corrected image, enabling complete use of primary radiation so physicians can achieve high-quality images with less dose. The development of innovative products like the digital full-field Mammomat Inspiration is a goal of the Siemens Healthcare Sector's global "Agenda 2013" initiative.
In digital X-ray breast imaging, radiation passes through the examined breast to a detector. Primary radiation supplies the information needed to produce the X-ray image, while scattered radiation is absorbed by special grids positioned between the breast and the detector. Unfortunately, these scatter grids also absorb part of the all-important primary radiation, forcing physicians to use a higher dose to obtain images of desired quality. Since mammography means regular screening of healthy women, minimizing dose is extremely important.
Siemens' new reconstruction algorithm for the Mammomat Inspiration system – known as Prime (Progressive Reconstruction, Intelligently Minimizing Exposure) – eliminates the need for the conventional scatter radiation grid. The Prime algorithm subsequently corrects the scattered radiation by identifying scatter-causing structures and recalculating the image. The primary radiation that radiologists rely upon remains intact. Therefore, a grid is no longer necessary, and lower doses are sufficient to produce high-quality images. The grid-free imaging technology of the Mammomat Inspiration Prime Edition can reduce radiation dose up to 30 percent compared to its predecessor model, depending on the thickness of the patient's breast tissue.
The software-driven Mammomat Inspiration Prime Edition demonstrates the innovative power of Siemens Healthcare and meets a goal of the global "Agenda 2013" initiative, which the Siemens Healthcare Sector unveiled in November 2011. The initiative defines plans of action to be implemented within two years in the areas of innovation, competitiveness, regional presence, and human resource development.
For press photos, please visit: www.siemens.com/healthcare-pictures/Mammomat-Inspiration.
The Siemens Healthcare Sector is one of the world's largest suppliers to the healthcare industry and a trendsetter in medical imaging, laboratory diagnostics, medical information technology and hearing aids. Siemens offers its customers products and solutions for the entire range of patient care from a single source – from prevention and early detection to diagnosis, and on to treatment and aftercare. By optimizing clinical workflows for the most common diseases, Siemens also makes healthcare faster, better and more cost-effective. Siemens Healthcare employs some 51,000 employees worldwide and operates around the world. In fiscal year 2012 (to September 30), the Sector posted revenue of 13.6 billion euros and profit of 1.8 billion euros. For further information please visit: http://www.siemens.com/healthcare
The products mentioned here are not commercially available in all countries. Due to regulatory reasons the future availability in any country cannot be guaranteed. Further details are available from the local Siemens organizations.
Tomosynthesis is not available in the U.S.
Reference Number: HCP201211004e
Henkestr. 127
91052 Erlangen
Germany
Tel: +49 (9131) 84-5337
This press release was updated on 11.12.2012 at 03:45 PM CET.