Industry Sector / Industry Automation Division
Nuremberg, Germany, 2011-Nov-15
The Siemens Industry Automation Division has equipped its modular, sector-independent Simatic WinCC/B.Data energy management system with new functions. The new Simatic WinCC/B.Data V5.2 SP1 version features a data connection wizard which facilitates easy and efficient linking of energy measuring points and WinCCarchive tags to B.Data. The wizard also supports the user in acquiring data from various sources such as WinCC, OPC or FTP. Installation is significantly faster and easier. Less experienced users are supported by default parameters, a standardized setup process, tooltips, simple configuration even for multi-user systems, as well as improved documentation. More experienced users benefit from the greater degree of freedom offered for selecting settings by the expert set-up mode. The new WinCC/B.Data version 5.2 SP1 not only supports WinCC V7.0 SP2 but also the supervisory control and data acquisition Scada system Simatic WinCC RT Professional V11 SP1, which is used to connect the energy management system to the runtime system of the TIA Portal engineering framework.
With the Simatic WinCC/B.Data energy management system, which now also supports Microsoft Excel 2010 and Windows 7, manufacturing companies can optimize their energy costs and transparency at management level, from purchasing to planning and controlling. Seamless energy and materials accounting in power generation and consumption systems enhances energy efficiency and lowers energy costs.
You can find more information on the Internet at: www.siemens.com/wincc
You can find this photo on the Internet at www.siemens.com/ia-picture/3105
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of innovative and environmentally friendly products and solutions for industrial customers. With end-to-end automation technology and industrial software, solid vertical-market expertise, and technology-based services, the Sector enhances its customers' productivity, efficiency, and flexibility. With a global workforce of more than 100,000 employees, the Industry Sector comprises the Divisions Industry Automation, Drive Technologies and Customer Services as well as the Business Unit Metals Technologies. For more information, visit http://www.siemens.com/industry
The Siemens Industry Automation Division (Nuremberg, Germany) supports the entire value chain of its industrial customers – from product design to production and services – with an unmatched combination of automation technology, industrial control technology, and industrial software. With its software solutions, the Division can shorten the time-to-market of new products by up to 50 percent. Industry Automation comprises five Business Units: Industrial Automation Systems, Control Components and Systems Engineering, Sensors and Communications, Siemens PLM Software, and Water Technologies. For more information, visit http://www.siemens.com/industryautomation
Reference Number: IIA2011113105e
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895-7945