Energy Sector / Power Transmission Division
Erlangen, Germany, 2009-Nov-27
Following successful final acceptance tests Siemens Energy will deliver the world’s largest and most powerful 800-kilovolt converter transformer in mid-January 2010. The world-record transformer produced at the Siemens manufacturing plant in Nuremberg is destined for the Xiangjiaba-Shanghai link, a high-voltage direct-current transmission link (HVDC) recently under construction. Spanning a distance of over 2000 kilometers and with a transmission capacity of 6400 megawatts (MW), this direct-current link is currently the longest and most powerful in the world. The HVDC link, which is scheduled to come on line in 2010, will connect the hydro power plants on the Jinsha river on the upper reaches of the Yangtze in central China with the coastal megacity Shanghai. Siemens will supply ten converter transformers, five of which are rated at 800 kV, for the Fulong converter station in the vicinity of the Xiangjiaba hydro power plant.
Siemens Energy will deliver the world’s largest and most powerful 800-kilovolt converter transformer in mid-January 2010. The world-record transformer produced at the Siemens manufacturing plant in Nuremberg is destined for the Xiangjiaba-Shanghai link, a high-voltage direct-current transmission link (HVDC) recently under construction. Spanning a distance of over 2000 kilometers and with a transmission capacity of 6400 megawatts (MW), this direct-current link is currently the longest and most powerful in the world.
“Thanks to our years of experience in the production of converter transformers and through innovative solutions in all key components we were able to increase the performance of our HVDC transformers by 25 percent. The transformers, which will be deployed for this 800-kV HVDC project, will therefore contribute toward sustainable, efficient power supply in China,” said Udo Niehage, CEO of the Power Transmission Division of Siemens Energy.
The single-phase 800-kV converter transformer scheduled for delivery is the first of five with a rated capacity of 321 MVA and a shipping weight of 380 metric tons. “With this transformer we’ve become best in class in this field of technology. Our whole range of products will benefit from the innovations implemented,“ said Jürgen Vinkenflügel, CEO of the Transformers Business Unit of Siemens Energy. The insulation systems of this high-tech transformer had to meet extremely stringent requirements. For example, the two valve-side bushings of the HVDC transformer are approximately 16 meters long because of the requisite insulation clearances. Furthermore, the dimensions specified by the carriers and the transformer’s shipping weight will call for superlative logistics achievements – for example, shipping by sea on a special heavy-load ocean-going vessel from Antwerp to Shanghai. For the State Grid Corporation of China, the future operator and the world’s largest utility with approximately one billion customers, the HVDC systems form the backbone of its power transmission network.
Energy-efficient high-voltage direct-current transmission technology (HVDC) is part of part of Siemens’ Environmental Portfolio. In fiscal 2009, revenue from the Portfolio totaled about €23 billion, making Siemens the world’s largest supplier of ecofriendly technologies. In the same period, our products and solutions enabled customers to reduce their CO2 emissions by 210 million tons.
Download press photo: www.siemens.com/Transmission/pictures/EPT200911020
The Siemens Energy Sector is the world’s leading supplier of a complete spectrum of products, services and solutions for the generation, transmission and distribution of power and for the extraction, conversion and transport of oil and gas. In fiscal 2008 (ended September 30), the Energy Sector had revenues of approximately EUR22.6 billion and received new orders totaling approximately EUR33.4 billion and posted a profit of EUR1.4 billion. On September 30, 2008, the Energy Sector had a work force of approximately 83,500. Further information is available at: www.siemens.com/energy.
Reference Number: EPT200911020e
Freyeslebenstr. 1
91058 Erlangen
Germany
Tel: +49 (9131) 18-4974