Industry Sector / Industry Solutions Division
Warrendale, Pennsylvania, USA, 2008-Nov-20
Siemens Water Technologies has established its mobile water treatment solutions in the Middle East with its first installation outside North America, where the company services thousands of municipal and industrial customers. Siemens will supply the system to Saudi Aramco in Saudi Arabia. The 50m3/hr system uses media filtration, followed by reverse osmosis, to treat and purify groundwater for use as drinking water. The mobile water treatment units began operation on June 15, 2008, and will be on site for about three years. Unlike other treatment systems, which require the investment of capital expense, manufacturing time, and installation, the containerized mobile water systems provide numerous advantages, such as rapid response for emergency or unplanned maintenance, minimal field construction costs and the flexibility to upgrade or change a treatment process if source water chemistry changes.
Containerized mobile water treatment system from Siemens Water Technologies.
The Siemens mobile water system at Saudi Aramco will supply 50 m3/hr of treated water to supplement an existing drinking water supply during construction of a new permanent system. The company selected a mobile unit instead of a permanent treatment system, because the fully integrated, containerized system can be installed quickly with minimal construction time. By using the Siemens water treatment system, Aramco has improved the quality and quantity of available drinking water from the existing wells. “The protection of this vital resource is an important responsibility and one of Saudi Aramco’s highest priorities,” said Mr. Mazen Snobar, Community Services Executive Director at Saudi Aramco. “We are greatly honored to work with Siemens Water Technologies, a leader in mobile water systems.”
Unlike the systems in North America which, are built inside trailers (on wheels), expansion of the mobile treatment concept into Saudi Arabia involved designing treatment systems to be built in international-standard ISO containers. All of the necessary interconnecting piping, power distribution, and instrumentation are complete within the container, including PLC controls for fully-automatic operations. Chemical feed systems are also integrated in the container, when required. This configuration allows Siemens to adapt fully-integrated treatment systems into transportable containers built to withstand rigorous use and transportation. Once on site, a single-point connection for water inlet and outlet and a single-point connection for the power supply are all that is required.
As part of the company’s new Middle East mobile services offering headquartered in Saudi Arabia, the mobile fleet is available in various treatment configurations, such as Pretreatment, Membrane Separation/Reverse Osmosis (RO) and Combination Pretreatment and RO. Mobile water treatment services provide temporary treatment solutions for short-term, emergency and supplemental water needs across a wide range of industrial and drinking water applications.
Further information about solutions for water treatment are available at
http://www.siemens.com/water
The Siemens Industry Sector (Erlangen, Germany) is the world's leading supplier of production, transportation and building systems. Integrated hardware and software technologies combined with comprehensive industry-specific solutions enable Siemens to enhance the productivity and efficiency of its customers in industry and infrastructure. The Sector comprises six Divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and Osram. In fiscal 2007 (ended September 30), Siemens Industry generated sales of approximately EUR40 billion (pro forma, unconsolidated) with around 209,000 employees worldwide. http://www.siemens.com/industry
With the business activities of Siemens VAI Metal Technologies, (Linz, Austria), Siemens Water Technologies (Warrendale, Pa., U.S.A.), and Industry Technologies, (Erlangen, Germany), the Siemens Industry Solutions Division (Erlangen, Germany) is one of the world's leading solution and service providers for industrial and infrastructure facilities. Using its own products, systems and process technologies, Industry Solutions develops and builds plants for end customers, commissions them and provides support during their entire life cycle.
Further information and downloads at:
http://www.siemens.com/industry-solutions
Reference Number: IIS200811.345e fp
Schuhstr. 60
91052 Erlangen
Germany
Tel: +49 (9131) 7-44544