Industry Sector / Industry Automation Division
Nuremberg, Germany, 2008-Oct-22
The Siemens Industry Automation Division has developed an all-inclusive kit for checking the performance and accuracy of any type and brand of energy meter in heating, ventilation and air conditioning applications.
The Siemens Industry Automation Division has developed an all-inclusive kit for checking the performance and accuracy of any type and brand of energy meter in heating, ventilation and air conditioning applications. The kit contains the clamp-on ultrasonic flowmeter Sitrans FUE1010 along with transducers, 1000 Ohm platinum resistance temperature detectors (RTD’s), cables, etc. required for measurement of district energy cooling and chilled water applications as well as power plants. Chiller efficiency analysis and surveys on non-metered installations can also be performed and be logged. The 2-channel flowmeter is built up for measurement on one or two pipes, enabling measurement on supply as well as return pipes with the use of only one meter. The 1 hour quick charge battery pack allows four hours of normal operation, ensuring facilitated field use and portability.
Further information can be found on the Internet at: www.siemens.com/flow
A photo accompanies this press release. You can find this photo on the Internet at: www.siemens.com/ad-picture/1651
The Siemens Industry Sector (Erlangen, Germany) is the worldwide leading supplier of production, transportation and building technologies. With integrated hardware and software technologies as well as comprehensive Industry-specific solutions, Siemens increases the productivity and efficiency of its customers in the fields of industry and infrastructure. The Sector consists of six divisions: Building Technologies, Industry Automation, Industry Solutions, Mobility, Drive Technologies and Osram. With around 209,000 employees worldwide Siemens Industry achieved in fiscal 2007 total sales of approximately EUR40 billion (pro forma, unconsolidated). www.siemens.com/industry
The Siemens Industry Automation Division (Nuremberg, Germany) is a worldwide leader in the fields of automation systems, low-voltage switchgear and industrial software. Its portfolio ranges from standard products for the manufacturing and process industries to solutions for whole industrial sectors that encompass the automation of entire automobile production facilities and chemical plants. As a leading software supplier, Industry Automation optimizes the entire value added chain of manufacturers – from product design and development to production, sales and a wide range of maintenance services.
Reference Number: IIA200808.1651
Gleiwitzerstr. 555
90475 Nuremberg
Germany
Tel: +49 (911) 895-7945