2013-Apr-09
Siemens does not just want to manufacture in Russia but also would like to expand its research activities. For example, with the steel producer Novolipetsk Steel, Siemens researchers at St. Petersburg State Polytechnical University are looking for special alloys for transformers, because with the right alloy, the "buzz" of a transformer station can be prevented. Scientists are investigating the properties of various metals and alloys.
Pictured: A researcher uses an electron microscope to investigate the microstructure of an alloy at St. Petersburg State Polytechnical University.
Reference Number: PN201305-07