2012-Jun-11
A special vehicle, traveling 60 kilometers per hour, transported these giants over a distance of 575 kilometers from the blade factory in Aalborg to the Danish town of Nakskov on Lolland Island. By car, the trip is about 330 km, but because of the length of the rotor blade some re-routing was necessary taking bridges and tunnels into consideration. In Nakskov the blades were painted – the painting cabin at the blade factory is currently limited to 58 m blade length.
Reference Number: PN201204-05