2013-Mar-05
Siemens Industry Automation Division is adding an especially powerful, versatile, and rugged CPU for the process industry to its Simatic controller family. Simatic PCS 7 CPU410-5H is currently the fastest and most powerful controller on the market and covers all applications, application scopes, and performance range with a single hardware and firmware platform. The CPU is supplied with the maximum configuration. According to the new dimensioning model, the user defines the performance required of the system using the expansion card to match the quantity framework and the size and type of application.
Reference Number: IIA2013033311-01