2013-Mar-05
For gesture and multi-touch operation, Siemens Industry Automation Division has come up with an industrial monitor with projected capacitive touch technology (PCT). Simatic IFP1900 MT is the first device of this type that the company has marketed and it expands its range of rugged HMI (Human Machine Interface) monitors with widescreen format. The device for built-in installation features a scratchproof 100% glass front with high resistance to chemicals and is offered with a 19-inch display diagonal. The highlights of the new industrial Flat Panels are the special industrial anti-glare surface and automatic detection of spurious touching and operator actions, for example, touching with the ball of the thumb or soiling.
Reference Number: IIA2013033309-01