2013-Apr-22
Three fully assembled Siemens high-speed Velaro D trains at the testing center in Wegberg-Wildenrath (PCW).
To date, the new train for German operator Deutsche Bahn has covered over 250,000 kilometers in test and licensing runs. Siemens is one of the world‘s leading manufacturers of high-speed trains. Velaro is one of the most reliable trains in all the countries in which it is deployed (26 trains in operation in Spain, 240 in China, eight in Russia, with eight more under construction). Velaro trains have already traveled over 150 million operational kilometers without a significant technical failure. In Spain and Russia, Siemens is also responsible for Velaro maintenance.
Reference Number: soaxx201313-01