2012-Nov-26
Siemens Healthcare introduced the new version (VA20) of its routine 3D and advanced reading software syngo.via, which was on display at the 98th Scientific Assembly and Annual Meeting of the Radiological Society of North America (RSNA) 2012 in Chicago. This new version features expanded mobile applications as well as enhanced functionality and additional applications. As an example, syngo.via now includes new applications for mammography reading and complex examinations in neurology, oncology, and cardiovascular diagnostics. Siemens also presented an entry-level software package for 3D visualization of computed tomography (CT) examinations. The new syngo.via version supports hospitals and practices enhance efficiency by means of IT, which is one of the goals of Siemens Healthcare's initiative Agenda 2013.
The picture shows syngo.Breast Care Reading, the standard client-server application for state-of-the-art mammography reading.
Reference Number: him201211002-02