March 16, 2010
With the Flender EMPP vertical mill drive the Siemens Drive Technologies Division has developed a drive concept that prevents load surges arising from short power supply interruptions and optimizes the transfer of forces between the drive and the mill. At the same time the number of components that may be susceptible to faults is reduced. This in turn increases plant availability, and enables the power range to be expanded to 15 MW.
Reference Number: IDT2010032313-01