2009-Dec-08
Prague, the capital of the Czech Republic, is also the centre of the country’s economic, political and cultural activity. It is home to one-tenth of the country’s population, and contributed around 24% of the Czech Republic’s GDP in 2007. Trade, tourism, transport and communications together made up one-third of Prague’s GDP in that year, while industry contributed only 13%, less than one-half of the national average shares of 32.6%, in one of the EU’s most industrialised economies. During the past 20 years of economic transition, Prague has seen a structural shift away from production and towards business-related services, and a number of multinational firms have their European headquarters in the city. Prague is ranked 24th overall in the European Green City Index, with a score of 49.78 out of 100. The city performs best in the categories of water, waste and land use, ranking in the top half of the index for these categories.
Reference Number: SOAXX20091222-24